STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1431 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Hot to do a discovery using Device authentiction

Did numerous builds using CubeIDE (10,000 lines of code). this error started coming up. "reason was unknown target"Got the following message:Make -j4 all  DriversSTM32L4xx_HAL_Driver/subdir.mk.91:  *** unable to generate command line.  stop.  "make  ...

JBonn by Associate III
  • 1507 Views
  • 1 replies
  • 0 kudos

Is license required to create product using SDMMC?

Is a license required to create commercial products using SDMMC?  I noticed there is support for it in cube IDE.  The SD Association indicates a yearly subscription requirement for creating even a host app that uses the SD standards. https://www.sdca...

RHale.2 by Associate II
  • 877 Views
  • 0 replies
  • 0 kudos

STM32IDE Toolchain using 2 Compiler in one Project

I would like to use 2 Compiler in one project, the old compiler for the bootloader, where addresses should not change for application and the other for the application to use a newer version.First I tried to select either or from the C/C++ Build -> s...

koster by Associate III
  • 1258 Views
  • 1 replies
  • 0 kudos

Hardfault Error While Debugging in Systemview

The SystemView is running properly when I don't integrate TouchGFX into STM32CubeIDE. However, when I integrate TouchGFX into my code, I'm able to debug with ST-Link. On the other hand, when I use J-Link, I'm getting a hardfault error while debugging...

Anil1472 by Associate II
  • 17150 Views
  • 9 replies
  • 1 kudos

Resolved! SPI Not communicating with aurdino

So , I wrote all driver my self so dont know how to ask this but i can provide you with few code.This is main.c file and other driver file is attached below........#include <string.h>#include "stm3f407xx.h"void delay(void){for(uint32_t i =0;i<500000/...

Resolved! Self initializing UART with Pin Stackign

Hello everyone,I have not conventional question. My purpose is to create code where 2 pins are used as two different interfaces (I2C1 and USART3). I know that pin Stacking option is just theoretical as no code is generated for this interface. I found...

MŻbik.1 by Associate II
  • 6308 Views
  • 5 replies
  • 3 kudos

Resolved! The end . bin file

Hi all,I plan to update my MCU. I would like to upload to MCU. bin file. If I understand correctly, this file can be uploaded entirely to the initial address of the MCU. It should not contain any extra data. I checked this file and just before the en...

Dabi by Associate
  • 1499 Views
  • 1 replies
  • 0 kudos