STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1439 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to attach debugger to an already running MCU ?

Hi,I'm using STM32CubeIDE with a SEGGER J-Link connected to an STM32F7.I manage to flash and debug the board but I can't find how to attach the debugger to the target without resetting it.Thank you for your help.HG

HGate.2 by Associate
  • 1588 Views
  • 2 replies
  • 0 kudos

Unavailable "Setting" tab and problem with make

Hi everybody!Have problem with building project, which is OK in TrueStudio. I have:Core/Inc/font24.o:(.rodata.Font24_Table+0x0): first defined herecollect2: error: ld returned 1 exit statusmake: *** [makefile:42: test3.elf] Error 1"make -j7 all" term...

EVoro.1 by Associate
  • 1641 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeIDE Project setup issue

When trying to create a Debugger configuration for a project opened from sources + Makefile, STM32CubeIDE fails to create the configuration and shows the following error messages:" Not able to get board target."" An internal error has occurred. Updat...

0690X00000Buf7sQAB.png
Romain1 by Associate III
  • 3519 Views
  • 6 replies
  • 0 kudos

Azure expansion hsm emulator

I'm working with a STM32F4 Discovery (413) eval board and working through bringing the device up on Azure IoT hub through various mechanisms. I've successfully (the firmware does not like being talked to from a Mac serial port, i've only had succes...

SBade.1 by Associate II
  • 720 Views
  • 0 replies
  • 0 kudos