STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 564 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! The end . bin file

Hi all,I plan to update my MCU. I would like to upload to MCU. bin file. If I understand correctly, this file can be uploaded entirely to the initial address of the MCU. It should not contain any extra data. I checked this file and just before the en...

Dabi by Associate
  • 1507 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIDE debug FreeRTOS queues

I am trying to view and debug the queues in my FreeRTOS project. To do this, I have to add the queues to registry with vQueueAddToRegistry. However, vQueueAddToRegistry takes an argument to a QueueHandle_t and in the project generated with STM32CubeM...

sute by Associate III
  • 3033 Views
  • 1 replies
  • 0 kudos

Not able to debug using ST Link

What might cause the attached in ST error message in Cube IDE (V 1.13.1.It used to be able to Deug my program, until i updated the STLink firmware ( Pop up prompted me to update), i tried uninstalling the IDE, installng it again, same error message.....

AHamad by Associate
  • 4098 Views
  • 4 replies
  • 1 kudos

How can I exclude a file from the .extsettings?

Hello Team,I am trying to use the .extsettings to handle my project structure in the stm32cubeIDE. I want to exclude a particular file from the list of source files that I have in my directory. However, I did not find any solution for this in the use...

Jansunil_0-1698050247275.png
Jansunil by Associate II
  • 1292 Views
  • 1 replies
  • 0 kudos

Project separation

I have a project for a STM32H7. The idea is to split the project into two separate projects. This is a functional separation. Can anyone help me what elementary steps are necessary to make these projects as follows:One project should land directly in...

DaBa by Associate
  • 1089 Views
  • 1 replies
  • 0 kudos

Build error log

I have recieved a project from a third party who was working on our source code. When I build, I get these errors. I am new to STM/Eclipse, so I am sort of lost on how to remedy the situation. Thanks!

MAlan.1 by Associate III
  • 1805 Views
  • 2 replies
  • 0 kudos

What is the point of this UI element?

When the project configurator will forever just generate a main.c and then never compile because 'class' type is not defined...Seriously STE... take a hint from this and below: Your IDE is bad and you should feel bad.  You have a UX, documentation, a...

capnhyaku_0-1697198402198.png

SWV ITM Data Console is empty

This problem is common, but I've reviewed my setup and everything appears to be correct, yet it still doesn't work.My programmer is an STLINK-V3PWR, connected via a 6 pin Tag-Connect (TVCC, SWDIO, NRST, SWCLK, GND, SWO) to an STM32F411CEU6.In the STM...

NateS by Associate III
  • 13157 Views
  • 14 replies
  • 1 kudos