STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1493 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 571 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32H755 dual core debugging problem

Good morning:Please I would like to receive your help.I am starting to learn to program the STM32H755 microcontroller using a nucleo board and the STM32CUBE IDE tools.My first project is to blink two leds using individual CPUs. That is, the green LED...

ST-LINK GDB server not work Reason: (0) Unknown.

HiI have this problem again..:C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.1.0.202305091550\tools\bin>C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externalt...

PZamb.2 by Associate III
  • 1033 Views
  • 0 replies
  • 0 kudos

Resolved! M2 Mac STM32IDE Error, The disk image couldn't be opened

Hi Everyone,I have a trouble issue and tried every solutions but they aren't working. Several times I tried to install stm32 cube ide I selected macos version but It doesn't work on my computer. I gave all permisions(read & write) still taking this p...

Screenshot 2023-11-15 at 23.01.11.png
BArsl.1 by Associate II
  • 2422 Views
  • 3 replies
  • 1 kudos

Recover .ioc file

Hi,Can I recover an .ioc file. The error message when i try to open it "Invalid State: Most probably trying to open 'file.ioc' file from an abnormal previous IDE session exit. Please close such editor and have a new try to recover properly."Thanks

kelseyy by Associate
  • 3894 Views
  • 3 replies
  • 1 kudos

Error in configuring USB CDC Class and UART in parallel on NUCLEO-F070RB using STM32 CUBE IDE

Dear ST Community,                                 I am currently facing an issue while configuring both USB CDC Class and UART in parallel on the NUCLEO-F070RB development board using the STM32 CUBE IDE. Specifically, I am encountering an error wher...

SANTHOSH1 by Associate II
  • 1283 Views
  • 0 replies
  • 0 kudos

No DNS options in LWIP->Key Oprions in IDE and MX

I am writing this in IDE section as I am using STM32CUBEIDE ver 1.13.1. In my project I wanted to connect to remote host (dynamic IP) by name. However with DHCP disabled (using static IP) and LWIP DNS enabled, there is no option to input DNS options ...

Rad Rad by Associate II
  • 2083 Views
  • 2 replies
  • 0 kudos

ST-Link v2 (OpenOCD) not work on STM32H7x

I want to use ST-Link OpenOCD to debug and program my STM32H7x board. But always got failure. My STM32CubeIDE version is STM32CubeIDE_1.13.2, .openocd_2.1.0.202306221132 is within CubeIDE. The attached is the config file for openOCD(.cfg is not allow...

HarryXia by Associate II
  • 6274 Views
  • 2 replies
  • 0 kudos