STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1557 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 590 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32CubeIDE for macOS 14.1, Sonoma

Hi all,I just updated STM32CubeIDE from version 1.13.1 to version 1.13.2. OK installation, but when I launch the App, the second splash windows shows up in a strange way, i.e. it is mirrored both horizontally and vertically, as visible in the attachm...

STM32F412G - Compile Error (STM32CubeIde)

Hi,For some strange reason projects that I have made that have compiled perfectly fine previously have started showing the below makefile  error message:-c:/st/stm32cubeide_1.12.1/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.make.win32...

Linkpad by Associate III
  • 1847 Views
  • 2 replies
  • 0 kudos

Resolved! LCD of STM3240G

Hi, I am trying to program the TFT LCD screen that is on STM3240G-EVAL MCU through STM32CUBEIDE. I just want to be able to put text onto it, or even a simple "Hello World program", but i cant get anything to display or find any tutorials. I'm not sur...

as2 by Associate
  • 2506 Views
  • 3 replies
  • 4 kudos

Problems with XOR on Bluepill (STM32F103)

Hi CommunityIt shouldn't be so difficult, but I'm having problems with the XOR function on CubeIde and a STM32F103 (Bluepill Board)I have this buffer:#define NUM_CHANNELS 17volatile uint16_t ihcData[NUM_CHANNELS]; I have these 2 functions that are wo...

SteenA by Associate III
  • 3438 Views
  • 0 replies
  • 0 kudos

Why does the index not work and how to make it work?

In STM32CubeIDE it seems that index don´t work. I tried refresh it, but it didn´t help. This happens when I import existing project into workspace. We tried it on multiple projects and multiple computers, but so far nothing has solved this problem

PŠirů.1 by Associate II
  • 12815 Views
  • 12 replies
  • 1 kudos

Resolved! ADC Triggered by Timer

Hello Team,In my application using STM32G431KCU6 at 160MHz, I want to trigger ADC2 channel by TIM1 channel. I aim to read ADC value synchronously with 1.1kHz pwm signal. When I set up the CubeMX config, i can see that TIM1 trigger OutputCompareCallba...

BKaya_0-1701065655338.png BKaya_1-1701065679267.png BKaya_2-1701065691737.png BKaya_3-1701065745458.png
B.Kaya by Associate III
  • 3686 Views
  • 1 replies
  • 1 kudos