STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1556 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 589 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! ADC value won't show voltage conversion

Currently in the process of coding an MQ5 gas sensor, right now I was able to get the ADC value to appear on the serial terminal using PuTTy, but for whatever reason the voltage value always produces zero. I tried also changing the formula to have it...

DRicc2_0-1703439555031.png
DRicc.2 by Senior
  • 3563 Views
  • 2 replies
  • 1 kudos

STM32CubeIDE stops working after waking up on debian/ubuntu

I've had this problem for months now, in Debian 12/13(and Ubuntu 20.04), if I suspend my PC while STM32CubeIDE(1.12 to 1.14, both generic linux and debian versions) is running, when I wake up the PC and log in, STM32CubeIDE is completely freezed, I d...

Tizio1234 by Associate II
  • 1707 Views
  • 1 replies
  • 0 kudos

STM32H7 HAL SPI DMA Not receiving data

I'm having a problem using DMA with SPI.Fault is almost certainly me as this is the first time I have used SPI/DMA.  Normally I just wait for SPI to finish, but on this occasion it is taking too long so I need to move the process away from the CPU wa...

STM32H7 with W5500 SPI DMA not working

My project requires me to make W5500 driver for ethernet. Everything works fine when using non-DMA. But as need to large data continuously, non-DMA is not ideal and need speed thus plan to use SPI DMA with W5500. In past, I had made successfully run ...

jain2051 by Associate
  • 3719 Views
  • 2 replies
  • 0 kudos

Resolved! ADC multi channel configuration(STM32F410)

Hello,I'm using STM32F410 for ADC in which i have configured two channels means two conversions.For IN7 channel the input voltage is 1.89V and for IN8 input voltage is 2.0v(This channel we have connected trimpot voltage can varied ) Please  check the...

Advance_tech_0-1702636700536.png Advance_tech_1-1702636828356.png

Resolved! STM32CubeIDE cannot find OpenSTLinux

I've set up the development environment for an STM32MP157F-DK2 kit including STM32CubeIDE. I'm following instructions to create a new application to run on the A7 under Linux, and CubeIDE cannot find the OpenSTLinux plugin. So I followed the instruct...

Bryan_H by Associate
  • 3255 Views
  • 2 replies
  • 0 kudos