STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1555 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 589 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Create Delay Function using STM32

I'm having trouble making the delay function in stm32f411vet. When the power frequency for the chip is 16MHZ, it still works normally but when the frequency is increased to about 64MHZ, the error occurs. Let me all ask you what fault this is.

dnk by Associate
  • 3945 Views
  • 3 replies
  • 0 kudos

Resolved! Project gives error even if nothing has changed

I have a problem on a new project I have never encountered before.  When I go to rebuild I aways get the following error for the same files or when I try to debug right after building:  make -j8 all make: stat: F:/Projects/Smart-Fly/PwrEq/MCUs/STM32/...

Problem updating to STM32cubeIDE 1.14.1

I presently have STM32CubeIDE 1.10.1 installed on my Windows 10 PC. It fails when I attempt to update to 1.14.0. Fig 1 shows the present version and Fig 2 shows the available updates and Fig 4 shows the error message. How do I get this to work? I wou...

Update Error.png

Resolved! Timer updates only after i set a breakpoint

I'm using an STM32F401RCT6 to create a very accurate millisecond timer for a school project. When the second interrupt of the alarm triggers i set a new CCR1 value and reset the timer. But it seems like the timer just ignores this. Only when i set a ...

Hesseltjuuh_0-1703784283302.png Hesseltjuuh_1-1703784292024.png Hesseltjuuh_3-1703784392779.png

Resolved! Can't start Debugging on STM32CubeIDE

I was working on my stm32f411re nucleo boards. i was using two of them with spi full duplex mode one as the master and the other one as the slave. I was working on my codes and at a certain point when i tried to debug one, it asked me to upgrade my s...

erincyldz_0-1703490146873.png
erincyldz by Associate III
  • 4652 Views
  • 5 replies
  • 0 kudos

OTA Update over serial communication

Hi,I am working on OTA update over serial port communication(UART) How can I achieve this?  How can I trigger the bootloader and download, install the firmware update.  As I am using stm32H563zi.  Can I get any reference for the above scenario.Thanks...

Monika_02 by Associate II
  • 3118 Views
  • 2 replies
  • 0 kudos

Having trouble interfacing RGB LED and Gas Sensor

Previously I posted on this forum as I was having trouble converting the gas sensor ADC value to voltage.That problem has since been fixed, although I seem to be running into a new issue where my WS2812 RGB LED won't turn on, and the PuTTy monitor is...

DRicc2_0-1703649644767.png
DRicc.2 by Senior
  • 1874 Views
  • 1 replies
  • 0 kudos

STM32F746G Discovery board

In STM32F746G Discovery board product Speifications, it is shown asSupport of a wide choice of Integrated Development Environments (IDEs) including IAR™, Keil®, GCC-based IDEs, and Arm® Mbed™But it has not given whether STM32CubeIDE works with it or ...

Moni by Associate
  • 1290 Views
  • 1 replies
  • 0 kudos

Resolved! Problem where fopen() a bitmap file returns "Not enough space"

Hello community, ■Problems occurring:When I tried to open a bitmap file with the fopen function as shown below, I encountered a problem that returned "Not enough space".Do I need to change any settings on the STM32CubeID side?Please help us solve it....

t-oka by Associate III
  • 6449 Views
  • 10 replies
  • 7 kudos