STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1087 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 470 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! syntax error but no compilation error

hello,I have a syntax error on one line but no compilation error with stm32cubeide 1.14.1HANDLE_busQuadSPI_CREATE(g_hbusQSPI_storage , &g_hqspi) ; //syntax error HANDLE_busSPI_CREATE(g_hbusSPI3_interne , &g_hspi3); // no syntax errorwith#define HAND...

po221 by Senior
  • 11267 Views
  • 19 replies
  • 4 kudos

chinese support in cubeIDE ?

I have been using CubeIDE as a development tool for many years.Compared to KeilMDK, it has a beautiful interface, powerful engineering management capabilities, and many helpful price differences.For example, the ctd completion plugin can greatly impr...

jlinker by Associate
  • 1501 Views
  • 0 replies
  • 0 kudos

Resolved! DAQ System on STM32F103 with fs 100kHz double channel

I need to implement a system with a real and fixed sampling frequency of at least 100kHz, using a STM32F103C8T6, for two analog signals. My main question is: what is the most optimal way to implement this system considering that I also need to do pro...

failed to start GDB server error

hello forum,I am getting following error - see picture https://i.imgyukle.com/2020/09/07/xXWynv.pngI use blue pill f103c8 - voltages are ok - blue pill is alive I can see the LED blinkoriginal st link v2 LED is red - driver is ok no error in device m...

STM32CubeIDE levelX Code Generation bugs

 Try to use LevelX customized Nor driver for STM32G0 in lastest release STM32CubeIDE 1.14.1When I regenerate code, whatever user code in lx_nor_driver_write() function will be copied to lx_nor_driver_block_erase() and lx_nor_driver_block_erased_verif...

Jackle by Associate III
  • 2146 Views
  • 1 replies
  • 0 kudos

Information about the content of RAM.ld file

Hi All,I notice that there are two linker files. One is called STM32F407VGT_FLASH.ld and the other one is called STM32F407VGTX_RAM.ld. When I check the content of ...FLASH.ld file, I see that there is a section for RAM as shown below.On the other han...

demir_0-1706455633192.png demir_1-1706455886094.png
demir by Senior II
  • 6162 Views
  • 2 replies
  • 0 kudos

Turn PWM on and off with a control variable

I'm using the STM32F103C8T6 microcontroller, better known as the blue pill.I need to make a code that reads the voltage of a port (which I already managed to do) and depending on the input voltage it turns the PWM on or off. I'm having trouble becaus...

Captura de tela 2024-01-26 124900.png Captura de tela 2024-01-26 125313.png Captura de tela 2024-01-26 125347.png

STM32CubeIDE - How To Include Flash Library Code?

HiForgive me for being dumb, but how do I include ST flash library code (functions to configure and program flash) in an STM32CubeIDE project?I expected to find it in the ioc device configuration tool, along with system core drivers (DMA/GPIO/IWDG et...

Resolved! header file can not be included in the build

Hi All,I am compiling my code, then I get the error below. As you can see, stm32f4xx.hal_can.h is included under project. But, when I click on open declaration for CAN_HandleTypeDef, it does not take me to the stm32f4xx.hal_can.h file. It is like the...

demir_0-1706431575259.png demir_1-1706431767698.png
demir by Senior II
  • 2045 Views
  • 1 replies
  • 1 kudos