User Activity

Hi, after of much struggle in the programming, seeing the tutorial of controllers_tech, can create files and directories in usb memory. I had problems with these case, when insert the usb memory the flow of program enter in Application_Start but neve...
I can configurate the touchGFX configurator with the stm32f746, i can open the .part and designer some figures and bottoms, these yes appears in the LCD, i use the hardware stm32f746 discoveryboard. But i no can active the function of the touch, have...
Hi i have configured the FMC and can read and write in SDRAM extern, begin in 0xC0000000, i now want create a variable in this SDRAM, then i define:uint32_t myFrameBuffer[65280] __attribute__((section(".sdram_data"))) = {0};but when i see the debugge...
Hi good day, i have a fanuc AC PMSM 140v, 6NM, 4.6A, 1kw, 2000ppri see the tool hardware and think what the follow kit is convenient:1.- Nucleo G431RB2.- X-nucleo IHM09M13.- STEVAL-IPM30Bbut i see MCSDK v6 no support this hardware, then I ask some ge...