STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Error in executing 'step' command in HAL_GPIO_Init

Hi Community,I am working on a stepper motor driver development board that uses SPI for configuration and a few GPIOs for control. The development board uses a 5V logic level and needs an interface to STM32G491RE. By referring to the datasheet I choo...

newbie_stm32_0-1708493856966.png newbie_stm32_1-1708493883071.png newbie_stm32_2-1708494023142.png newbie_stm32_3-1708494056497.png

Regenerated Code

Hi everyone!I use STM32CubeIDE and the RTC of my uC. Everytime I change something on STM32CubeMX the code is regenerated and I know that I must write my personal code in the USER SECTIONS. My question is that I want to change parameters in the initia...

my init.png RTC init.png
Fannyrsy by Associate II
  • 2714 Views
  • 3 replies
  • 0 kudos

Live expressions not showing

I have a problem with showing live expressions. They worked on a previous project but now that I created a new one and copied the code to it, they are not showing anymore.Any idea what could be the issue?

_legacyfs_online_stmicro_images_0693W00000bi5BAQAY.png
PPopo.1 by Senior
  • 2790 Views
  • 2 replies
  • 0 kudos

Resolved! memory dump to a file

Hello,Using CubeIDE v1.14.1, I would like to download memory to a file, for import into a worksheet, etc.  But I've not located the ability to do that, via the IDE menus.  Is there such a capability?  I'm initially dealing with floating point values,...

R_DSP by Associate II
  • 11880 Views
  • 4 replies
  • 0 kudos

Output compare mode.

Good afternoon community,I am traying to Output compare unit on STM32F407G Discovery.  I am configuring TIM1 and generate with global interrupt. Here is timer configuration function.This is Callback Function.//Callback function void HAL_TIM_OC_DelayE...

MG1 by Associate II
  • 1695 Views
  • 1 replies
  • 1 kudos

I cant display the value via UART.

Hi,I wrote an application as below which prints formatted values. However, when I print the Adc.IntSensTmp, I dont see the value as expected. Instead, I see the output below. Could you pls help me resolve ?Thanks. Here is the output I get.   

demir_0-1708283156485.png demir_1-1708283178472.png demir_2-1708283202000.png demir_3-1708283299424.png
demir by Senior II
  • 1378 Views
  • 3 replies
  • 0 kudos

STMCubeIDE running previous build before running latest build

Basically what I said in the title. After rebuilding and running, it first runs the most recent previous build and then after a few seconds, the newest build.I even made a new project from scratch but I get the same result.I am using an STM32F411RE. ...

Hermie by Associate
  • 1419 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIDE cloning (copying) a project

A usual approach is to branch from a given project by making a copy of it and develop further on the copy, leaving the original intact. How can this be achieved in the STM32CubeIDE project tree?I tried it by copying the directory in the filsystem, to...

chriskuku by Senior III
  • 18986 Views
  • 14 replies
  • 9 kudos

Resolved! what is the purpose of -1 at HAL_UART_Transmit ?"

Hi,I copied below code from internet which works perfect while using HAL_UART_Transmit. However, I want to understand more why there is minus 1 (-1) at timeout parameter ?P.S.: This question may not be directed at the right section, apologies for tha...

demir_0-1708271235831.png
demir by Senior II
  • 1438 Views
  • 1 replies
  • 1 kudos