STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 561 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Clock Circuitry

BYPASS Clock SourceThe above is the setting, that I give in the Clock Configuration. It simply bypasses the PLL Circuit. But I want to know, what happens internally in this circuit. How this bypass happens internally is my question.?If anyone, know p...

PLL_bypass.png

Resolved! Miscellaneous bit field arrangement in STM32G4

Hi Community,I have a bitfield arrangement for one of the driver files which is a 32-bit value. While debugging I was not able to figure out how it is being stored in the register. The bit order and endianness are not always guaranteed in structs and...

Scan my code for vulnerabilies using STMCubeIDE

I am tasked to scanned the C code for vulnerabilities using source analyzer.I am wondering is there a possibilities of add external tool such as the source-analyzer to the IDE to perform the scanning?Best Regards 

How to compile this code on a Nucleo

H! I am trying to compile this program in a Nucleo (the source code is build for the specific version of the Nucleo that I am using) using STM32CubeIDE but the result on the console is Program “make” not found in the path. 

IMG_0949.jpeg
ATeli.1 by Associate III
  • 2975 Views
  • 5 replies
  • 1 kudos

Resolved! CMake project debugging C++ problem

I'm wondering with implementation of CMake into stm cube.I tried default project executable and it works for C and I'm able to debug it.But if I change it to C++ I'm unable to debug it. Program always jumps to this line:Infinite_Loop:b Infinite_Loop....

Peterko by Associate
  • 3841 Views
  • 2 replies
  • 1 kudos

Resolved! STM32CubeIDE + FreeRTOS + LWIP

Does anyone know what is causing this error and how to fix it in STMCubeIDE?  As shown, this is specific to STM32F107VCT as it may be that STM32F4 does not see this. Buildable code cannot be generated.Thanks!@Amel NASRI 

spoatech_0-1709573051963.png
spoatech by Associate II
  • 5466 Views
  • 9 replies
  • 0 kudos

X-CUBE_STL-G4 installing problem

Respected all,i am actually trying to implement STL for a project for checking ram, cpu health in precise the package is X-CUBE_STL-G4 so the files i got from the vendor are  package license _htmrescdrivers middlewaresfew projectsrelease notesuser gu...

snewkar by Associate II
  • 3167 Views
  • 4 replies
  • 0 kudos