STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Delayed in PWM and interrupt

HiI'm implemented the most simple pwm generation and using interruptions in F401RE with TIM1. But a delay has been in the PWM generation and the update event interrupt (underflow and overflow) the most large pulse is the PWM and the another the when ...

Resolved! New STM32Project that uses Low Level drivers

STM32CubeIDE 1.12STM32G0B0RE microWe have an older Cube project from a STM32F0 series that needs to be changed to the larger STM32G0B0 chip. We thought that we would just create a new project with the new micro and port in the older code. When we cre...

0693W00000bhPzwQAE.jpg

Resolved! azure rtos on stm32h5

Hi, is there support of azure rtos for stm32h5 devices?I am looking for a MCU with ethernet and azure rtos support. I have fond some examples for sym32h7 devices but those are too big. Smallest is 100pins and they are more expensive. The smallest and...

PR.10 by Senior
  • 1898 Views
  • 1 replies
  • 0 kudos

Resolved! NetXDuo and ThreadX : Increasing number of TCP Server response

Dear Experts,I’m currently working on a project involving an STM32 board (B-U585I-IOT02A). I would like to use this board as a TCP Server . Therefore, from the STM32CUBEIDE application, I had observed that there is an example project in which it is p...

Nicolas_G_0-1708684494529.png Nicolas_G_1-1708684574247.png Nicolas_G_2-1708685721604.png
Nicolas_G by Associate II
  • 8412 Views
  • 5 replies
  • 2 kudos

I can not activate the Ethernet

Hi everyone,I have a NUCLEO-H745ZI-Q board. I try to activate ethernet, but I could not. I watched videos, read tutorials, post about it. Firstly, I thought it was my mistake. I must have made a mistake somehere, so I downloaded stm32 ethernet exampl...

code generator not work

when i try to generate "main.h" saving all after select "generate peripheral", in the window outline dont appear anything, i dont have any codei dont know how to fix it 

Manuel13_0-1710216769517.png
Manuel13 by Associate II
  • 2146 Views
  • 4 replies
  • 0 kudos

eclipse error "Lauching 'MEMS' has encountered a problem...

Hi,I remember now, why I've never liked Eclipse... I've done some tests SW with my new STM32F4-Disc1 board and tried to get the initial gyro demo running again.For this I tired to install the MEMS lib (Middleware & SW Packs) and after that I cannot c...

bkneer_0-1710694051224.png
bkneer by Associate II
  • 881 Views
  • 0 replies
  • 0 kudos

Resolved! Problem with STM32 VSCode Extension

I have an issue with adding files to a project I have using the STM32 VSCode extension. I have been working on this project for some time without issue. However, today I needed to add a new source file, I opened STM32CubeIDE and added the source file...

SidPrice by Associate III
  • 2510 Views
  • 1 replies
  • 1 kudos