STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32H755 Nucleo M4 core debugging problem.

Hello, STM32 community,I am currently working on a project using the STM32H755ZI-Q Nucleo board, and I've encountered a perplexing issue with the M4 core during debugging. I have written a basic code to toggle two onboard LEDs, and while the code see...

shubham_patayane_0-1706572107481.png shubham_patayane_2-1706572362995.png

Application ofsset causes a error for loading into flash

Hello all, i am trying to make an offset for my application to have a start of flash for bootloader. So i set up an offset in linker file, so instead of 0x08000000 to 0x0804B000 and vector table offset during startup. But the problem is that i am una...

Eiffel_0-1710361179706.png Eiffel_1-1710361394041.png Eiffel_2-1710361623881.png
Eiffel by Senior
  • 2374 Views
  • 4 replies
  • 0 kudos

Could some expert on STM32F4 series explain the meaning of the following message on my CubeIDE Debugger Console. It was all fine till now, suddenly, this error and program aborts

Note: automatically using hardware breakpoints for read-only addresses.set *(int *)0xE000EDFC=*(int *)0xE000EDFC|0x7F0Program received signal SIGTRAP, Trace/breakpoint trap.0xfceaf000 in ?? ()

NAnand1 by Associate III
  • 6870 Views
  • 8 replies
  • 7 kudos

Resolved! STM32CubeIDE/ Cant add library to project file

Hi all,Im having problems with my IDE, I cant seem to add the stm32f407xx.h library to my project, which is an internal library provided by ST. I added it to the linker GCC both the path to the file directory and the file itself and its still not acc...

ADyankov_0-1710402239705.png
ADyankov by Associate II
  • 7389 Views
  • 14 replies
  • 1 kudos

Resolved! STM32H573I-DK CAN Support

Hi, is there CAN support available in STM32H573I-DK board, when I check STM32H573I-DK datasheet 2 CAN FD is mentioned. but pin io details are not available in user manual.  

saran1 by Associate
  • 1770 Views
  • 2 replies
  • 3 kudos

Resolved! stm32h5xx_hal_usart.h is missing

I create a project by selecting the NUCLEO-H563ZI and answer yes to the question about initializing peripherals and the project will not build.  The error is: file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,from ../Drivers/S...

CubeMX Blank tab within CubeIDE

Hello,when i click on a .ioc file within CubeIDE, CubeMX is opened inside of CubeIDE. It starts opening the ioc file and shows progress bars: But then, after opening, it shows only a tab with no content.Does someone know whats wrong here? I use:Debia...

forum_1.png forum_2.png
sk-st by Associate III
  • 1781 Views
  • 2 replies
  • 0 kudos

Data mismatch found at address 0x0C000004

Whilst using the Trustzone examples given for the NUCLEO-WBA52cg BoardTx_SecureLEDToggle_TrustZone  RTC_TrustZoneCORTEXM_InterruptSwitch_TrustZone im encountering the error:Error: Data mismatch found at address  0x0C000004 (byte = 0xF9 instead of 0x8...

Isko by Associate II
  • 2388 Views
  • 3 replies
  • 0 kudos