cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L452CE CubeIDE Linker script causes hardfault inside Reset_Handler

jeremyh
Associate II

Hi,

Here is the default linker script that is generated by CubeIDE 1.14.0 for the STM32L452CEU:

/*
******************************************************************************
**
** @file        : LinkerScript.ld
**
** @author      : Auto-generated by STM32CubeIDE
**
** @brief       : Linker script for STM32L452CEUx Device from STM32L4 series
**                      512KBytes FLASH
**                      160KBytes RAM
**                      32KBytes RAM2
**
**                Set heap size, stack size and stack location according
**                to application requirements.
**
**                Set memory bank area and size if external memory is used
**
**  Target      : STMicroelectronics STM32
**
**  Distribution: The file is distributed as is, without any warranty
**                of any kind.
**
******************************************************************************
** @attention
**
** Copyright (c) 2024 STMicroelectronics.
** All rights reserved.
**
** This software is licensed under terms that can be found in the LICENSE file
** in the root directory of this software component.
** If no LICENSE file comes with this software, it is provided AS-IS.
**
******************************************************************************
*/

/* Entry Point */
ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */

_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */

/* Memories definition */
MEMORY
{
  RAM    (xrw)    : ORIGIN = 0x20000000,   LENGTH = 160K
  RAM2    (xrw)    : ORIGIN = 0x10000000,   LENGTH = 32K
  FLASH    (rx)    : ORIGIN = 0x8000000,   LENGTH = 512K
}

/* Sections */
SECTIONS
{
  /* The startup code into "FLASH" Rom type memory */
  .isr_vector :
  {
    . = ALIGN(4);
    KEEP(*(.isr_vector)) /* Startup code */
    . = ALIGN(4);
  } >FLASH

  /* The program code and other data into "FLASH" Rom type memory */
  .text :
  {
    . = ALIGN(4);
    *(.text)           /* .text sections (code) */
    *(.text*)          /* .text* sections (code) */
    *(.glue_7)         /* glue arm to thumb code */
    *(.glue_7t)        /* glue thumb to arm code */
    *(.eh_frame)

    KEEP (*(.init))
    KEEP (*(.fini))

    . = ALIGN(4);
    _etext = .;        /* define a global symbols at end of code */
  } >FLASH

  /* Constant data into "FLASH" Rom type memory */
  .rodata :
  {
    . = ALIGN(4);
    *(.rodata)         /* .rodata sections (constants, strings, etc.) */
    *(.rodata*)        /* .rodata* sections (constants, strings, etc.) */
    . = ALIGN(4);
  } >FLASH

  .ARM.extab   : {
    . = ALIGN(4);
    *(.ARM.extab* .gnu.linkonce.armextab.*)
    . = ALIGN(4);
  } >FLASH

  .ARM : {
    . = ALIGN(4);
    __exidx_start = .;
    *(.ARM.exidx*)
    __exidx_end = .;
    . = ALIGN(4);
  } >FLASH

  .preinit_array     :
  {
    . = ALIGN(4);
    PROVIDE_HIDDEN (__preinit_array_start = .);
    KEEP (*(.preinit_array*))
    PROVIDE_HIDDEN (__preinit_array_end = .);
    . = ALIGN(4);
  } >FLASH

  .init_array :
  {
    . = ALIGN(4);
    PROVIDE_HIDDEN (__init_array_start = .);
    KEEP (*(SORT(.init_array.*)))
    KEEP (*(.init_array*))
    PROVIDE_HIDDEN (__init_array_end = .);
    . = ALIGN(4);
  } >FLASH

  .fini_array :
  {
    . = ALIGN(4);
    PROVIDE_HIDDEN (__fini_array_start = .);
    KEEP (*(SORT(.fini_array.*)))
    KEEP (*(.fini_array*))
    PROVIDE_HIDDEN (__fini_array_end = .);
    . = ALIGN(4);
  } >FLASH

  /* Used by the startup to initialize data */
  _sidata = LOADADDR(.data);

  /* Initialized data sections into "RAM" Ram type memory */
  .data :
  {
    . = ALIGN(4);
    _sdata = .;        /* create a global symbol at data start */
    *(.data)           /* .data sections */
    *(.data*)          /* .data* sections */
    *(.RamFunc)        /* .RamFunc sections */
    *(.RamFunc*)       /* .RamFunc* sections */

    . = ALIGN(4);
    _edata = .;        /* define a global symbol at data end */

  } >RAM AT> FLASH

  /* Uninitialized data section into "RAM" Ram type memory */
  . = ALIGN(4);
  .bss :
  {
    /* This is used by the startup in order to initialize the .bss section */
    _sbss = .;         /* define a global symbol at bss start */
    __bss_start__ = _sbss;
    *(.bss)
    *(.bss*)
    *(COMMON)

    . = ALIGN(4);
    _ebss = .;         /* define a global symbol at bss end */
    __bss_end__ = _ebss;
  } >RAM

  /* User_heap_stack section, used to check that there is enough "RAM" Ram  type memory left */
  ._user_heap_stack :
  {
    . = ALIGN(8);
    PROVIDE ( end = . );
    PROVIDE ( _end = . );
    . = . + _Min_Heap_Size;
    . = . + _Min_Stack_Size;
    . = ALIGN(8);
  } >RAM

  /* Remove information from the compiler libraries */
  /DISCARD/ :
  {
    libc.a ( * )
    libm.a ( * )
    libgcc.a ( * )
  }

  .ARM.attributes 0 : { *(.ARM.attributes) }
}

 

This linker script causes a hardfault immediately (on the second instruction executed), presumably because the stack pointer is bad:

Leakster_Xubuntu_64-bit_22_04_2.png

 

The RAM size in the linker script is by default set to 160K, however, the size of SRAM bank 1 is actually 128K. Changing the map fixes the issue:

MEMORY
{
  RAM    (xrw)    : ORIGIN = 0x20000000,   LENGTH = 128K
  RAM2    (xrw)    : ORIGIN = 0x10000000,   LENGTH = 32K
  FLASH    (rx)    : ORIGIN = 0x8000000,   LENGTH = 512K
}

(the RAM1 size has been reduced to 128K)

However, this is discarding 32K of SRAM. Also note that if you look in the L452 examples in the ST github repo, it also only maps 128K RAM: https://github.com/STMicroelectronics/STM32CubeL4/blob/master/Projects/NUCLEO-L452RE/Examples/GPIO/GPIO_IOToggle/STM32CubeIDE/STM32L452RETX_FLASH.ld

_estack = 0x20020000;    /* end of RAM */

... snipped ...

MEMORY
{
RAM1 (rw)      : ORIGIN = 0x20000000, LENGTH = 128K
RAM2 (xrw)      : ORIGIN = 0x10000000, LENGTH = 32K
FLASH (rx)      : ORIGIN = 0x8000000, LENGTH = 512K
}

I'm not entirely sure why the stack can't be placed in SRAM2 even though it is supposed to be mapped contiguously with SRAM1. This seems to be undocumented in the errata.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Souhaib MAZHOUD
ST Employee

Hello @jeremyh 

After checking internally, this is a known issue that has been tracked with this ticket 173165 that will be fixed asap.

THX

Souhaib

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Souhaib MAZHOUD
ST Employee

Hello @jeremyh 

Thank you for bringing this issue to our attention, I will check it internally and get back to you as soon as possible.

Thx

Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Souhaib MAZHOUD
ST Employee

Hello @jeremyh 

After checking internally, this is a known issue that has been tracked with this ticket 173165 that will be fixed asap.

THX

Souhaib

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.