STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

RIVERDI H757 dual core from TouchGFX to CubeIDE

Hi there!My goal is to use the RIVERDI example provided in Touch GFX and import it into the CubeIDE to add some peripherial features as ADC and CANFD. When the .ioc file is imported into CubeIDE all the generated folders are empty and even the .ioc f...

PGrif2_2-1715586427167.png PGrif2_4-1715587124534.png PGrif2_0-1715585901208.png PGrif2_1-1715586078883.png
PGrif.2 by Associate III
  • 2170 Views
  • 2 replies
  • 0 kudos

Not able to flash stm32g030c8t6 with st link v2

-------------------------------------------------------------------STM32CubeProgrammer v2.16.0-------------------------------------------------------------------   Log output file: C:\Users\adity\AppData\Local\Temp\STM32CubeProgrammer_a09404.logST-LI...

Resolved! How to open "Live expressions" tab?

I have accidentally closed this tab (with X) so it no longer shows in my debug tabs, and can't find where is the setting to re-add it :(I'm using Cube version 1.10.1

"stm32cubeidec -build all" results to extra build runs

I have tried to build an example STM32H7Cube project with a command line script (attached) and got that the each CM7 and CM4 project configuration is built twice: the "Release" for CM7 is built twice, then the "Debug" for CM7 is built twice, and then...

ERROR by Senior
  • 946 Views
  • 0 replies
  • 1 kudos