cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 6.11.1 & CubeIDE 1.10.1 CMIS_OS2.h OS_TICK.H drivers errors

debugging
Lead

Building simple project (just enabling UART and XTAL OSC) SMT32F401CCU6 project generates this error.

Have been using STMcubeMX/IDE for years, but never encountered this with the UDE.

MX and IDE have been updated the the latest version

none-eabi-gcc "../Drivers/CMSIS/RTOS2/Source/os_systick.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32F401xC -c -I../Core/Inc -I../Drivers/STM32F4xx_HAL_Driver/Inc -I../Drivers/STM32F4xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/CMSIS/RTOS2/Source/os_systick.d" -MT"Drivers/CMSIS/RTOS2/Source/os_systick.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/CMSIS/RTOS2/Source/os_systick.o"
In file included from ../Drivers/CMSIS/RTOS2/Template/cmsis_os1.c:28:
../Drivers/CMSIS/RTOS2/Template/cmsis_os.h:157:10: fatal error: cmsis_os2.h: No such file or directory
157 | #include "cmsis_os2.h"
| ^~~~~~~~~~~~~
compilation terminated.
../Drivers/CMSIS/RTOS2/Source/os_systick.c:25:10: fatal error: os_tick.h: No such file or directory
25 | #include "os_tick.h"
| ^~~~~~~~~~~
compilation terminated.
make: *** [Drivers/CMSIS/RTOS2/Template/subdir.mk:19: Drivers/CMSIS/RTOS2/Template/cmsis_os1.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [Drivers/CMSIS/RTOS2/Source/subdir.mk:25: Drivers/CMSIS/RTOS2/Source/os_systick.o] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

After installing 1.15 thing went back to normal. The errors disappeared (no code or any changes).... Not sure why...

View solution in original post

2 REPLIES 2
debugging
Lead

Hmm CubeIDe seems on version 1.15 now. Always used the update it using the IDE update function but that did not update, so did not notice the latest version

After installing 1.15 thing went back to normal. The errors disappeared (no code or any changes).... Not sure why...