User Activity

The TF-A Makefile.sdk creates a small metadata.bin file for each type of boot (USB, SD-cARD, EMMC)1/ How to generates this outside of Makefile.sdk  ? I use this, but is only generates one file and there seems no parameter for the type of the boot dev...
Same or related postshttps://community.st.com/t5/stm32-mpus-products/op-tee-error-on-new-v5-0-0-sdk/td-p/578239/page/2https://community.st.com/t5/stm32-mpus-products/op-tee-error-tzc-permission-failure-on-new-v5-0-0-sdk/m-p/584339Custom STM32MP157AAA...
On STM32MP1 discrete power.  512MB DDR , TF-A & OPTEE configure in SYSRAME/TC:0 0 Panic at core/arch/arm/plat-stm32mp1/cpu_opp.c:106 <set_clock_then_voltage>Log attached.This message seems to unique for stm32mp1 in OP-TEE  code. no other platform sou...
Custom STM32MP157AAA3 board with 512MB DDR.[Note: the NOTICE: DEBUG messages in below logs were added to the source code of TF-A]The TF-A DT was compiled with option for SYSRAM with resulting dtb fw-configOP-TEE was compiled for SYSRAM and and enable...
Using the latest CubeMX 6.9.0 on Ubuntu  23.04  The following has happened quite a few times in the past years , also on  previous Linux and CubeMX versions. Now would like to raise this  issue as it's becoming very annoying now doing more work in Cu...