STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1418 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! fatal error #.elf: No such file or directory in STM32CubeIDE

Hello,I’m trying to build the tutorial project at https://www.micropeta.com/video43 using STM32CubeIDE , I’ve tried it for the stm32f103c8t6 and it builds without error but when I tried to debug it said that these no such dt.elf file or directory. I ...

440802817_1268568877437770_877855977088048128_n.png 445380639_7993749150649677_997007857836132722_n.png
kathus by Associate II
  • 5086 Views
  • 9 replies
  • 0 kudos

Couldnot reconstruct chunks at receiver end

Hello!I am doing a project using STM32cube ide , the problem I am facing is at the receiver end when the data at the transmitter is transmitted in form of chunks but at the receiver end, the received data could not reconstruct , the receiver is takin...

SVW console - no output after few seconds

I am using SWV ITM console (printf output) and SWV Data Trace Timeline Graph. They works only few seconds and then no output, while the program still works (LEDs reacts on interrupts, etc.) only no SWV debug outputs are provided.I am using STM32G474R...

ondra by Associate
  • 1786 Views
  • 2 replies
  • 0 kudos

Fault analyzer toolbar missing

Hello everybody,Since I did last update of STM32CubeIDE software I cannot see the fault analyzer toolbar anymore (attached file img).Am I missing some configuration to display it?Or is due to the update?Thank you for your time 

lucius92 by Associate
  • 4211 Views
  • 5 replies
  • 0 kudos

B-U585-IOT02A BSP example issues

Hello forumI have just purchased the B-U585-IOT02A and would like to start and interact with all of the sensors on in,for it, I tried the IDE example of the BSP in general, but it didn't even compile. even after trying to manually use the driver noth...

Resolved! CubeIDE linked list code generation error

Hi all,I'm using STM32Cube IDE (version 1.15.1 Build: 21094_20240412_1041 (UTC)) and have the STM32H573 chip with the LinkedList feature.Unfortunately the code generation of the linked list does not work properly and forgets to set some config settin...

joker_0-1716281151165.png
joker by Associate
  • 1615 Views
  • 1 replies
  • 1 kudos