User Activity

Any news on when there will be an update to CubeIDE to better support macOS Sequoia?At the moment we need to use a terminal launch hack to get support for debug tools. Would be nice to get a fix for this soon.
Steps to reproduce: Start a new STM32 Project in STM32CubeIDE v1.17.0Select NUCLEO-F746ZG board, and initailize all peripherals.Now in the IOC editor, under Middleware select LwIP and enable it.Set the PHY to LAN8742 in the "Platform Settings" tab.On...
I am debugging an application for an STMF103RCTX Using STM32CubeIDE and an STLINK v2 debugger.This is my usual combination of tools and my usual hookup.I find that I can start a debug session and step into main() and even step over anything befoer HA...
If I call HAL_UARTEx_ReceiveToIdle_IT to receive 512 bytes, will it wait till all 512 bytes are received before calling HAL_UARTEx_RxEventCallback or could it possibly call it several times, delivering fragments of the whole packet?I'm asking because...
My setup is macOS 15.0 SequoiaSTM32CubeIDE 1.16.1STLink-Server v2.1.1When trying to program or debug a device the following error is shown:Even after re-installing ST-Link serverI have rebooted and re-installed ST-Link Server, but the issue persists....