I have a TFT display which outputs 320 X 240 pixels and I want to control the display brightness from the command itself which I found in the datasheet of the TFT display controller IC, so with the reference from the datasheet I have to trigger the W...
I have F407G Disc1 board where it has the SWD ports and I want use this board as a standalone external debugger and I went through the manual for the connections but got stuckAlso found a thread in stack exchange where the connections are given as be...
I have STM32F series board and I'm using the ADC how can I give the input from a function generator to the board and get the digital output values on the STM32Cube IDEPS: I'm using STM32cube IDE 1.7.0