STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1405 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STMCubeIDE does not create links to SPI HAL files

I am starting to use the H755Zi Nucleo board. I have been using the F767Zi and F746Zg prior to this and familiarity with STM32CubeIDE. I see that there are no examples for the H755Zi-Q, but there are for the H745Zi-Q and do seem to run on the 755 boa...

jdw by Associate II
  • 1899 Views
  • 2 replies
  • 0 kudos

LSM6DS example and dev. board.

Hello, does anybody know what example and development board to use for LSM6DS for air mouse development?And is LSM6DS the best sensor to use?

GS2 by Senior II
  • 883 Views
  • 0 replies
  • 0 kudos

Resolved! Rename the project does not rename the .ic file

I wanted to use the ioc and all the code from a project into another project. So, I copied the project and pasted in a workspace, then renamed the project, but ioc is not changed. So while opening, I get error messageInvalid Input: Must be project's ...

Techn by Senior III
  • 2276 Views
  • 3 replies
  • 1 kudos

STM32CubeIDE BUG with working CMake project

Hello,I have a working project based on CMake.I tried to build it under STM32CubeIDE with no success.Here is the output when trying to build the project:**** CMake Configure of configuration config_default for project CMakeProject **** C:\Work\Projet...

ANauz.1 by Senior II
  • 1655 Views
  • 1 replies
  • 0 kudos

STUSB1602 + STM32F446ZE

I am currently working on a project where USB-C PD stack implementation on STM32F446ZE board. I have downloaded the necessary files which I have shown in my attachment (zip folder downloaded from https://github.com/usb-c/STUSB1602). Kindly answer my ...

Disassembly view buggy?

This is using Stm32CubeIDE  Version: 1.14.0 Build: 19471_20231121_1200 (UTC)When I hit a breakpoint that says "view disassembly" that button often goes to a blank disassembly view. Same if you try and go to a particular address.  If you close the cur...

musmuris by Associate II
  • 4206 Views
  • 5 replies
  • 1 kudos

Unavailable FW package issue (fixed)

Dear STM32CubeMX/STM32CubeIDE users We detected an issue linked to unavailability of some Cube packages for multiple STM32 series. This misbehavior is caused by an issue in the published database used by our tools. The issue is currently under invest...