STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1405 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32_modbus issues

Can anyone suggest me what the issues in the below code, i had generated the Modbus data frame and also checked the CRC function with Modbus- CRC calculator, I am able to transmit the data and also i am also waiting for the data to receive on interru...

Resolved! x-cube-cryptolib

Good evening,Could you help me install the x-cube-cryptolib library in STM32CubeIDE? I have tried everything and I still can't install it correctly. I would greatly appreciate your help.

Zero-96 by Associate II
  • 1743 Views
  • 2 replies
  • 1 kudos

Resolved! Cubeide does not start (and 'Spawner Reaper')

I installed cubeide (under linux ver 1.15.1) and started it by creating a workspace.I created a new project (STM32 project), the 'Target selector' appeared and I selected the nucleo-g474re board.I gave the project a name, I answered yes to the questi...

STM32CubeIDE cannot start my app for STM32F103RC.

hi, all. I made my app with STM32CubeMX for STM32F103RC(of custom board).I compiled with STM32CubeIDE(ver. 1.15.1), but cannot start in IDE. (refer to the atached file.)But after power off/on board, my app works fine.My app is simple, has just one LE...

mcu-down.png
yangbh by Associate II
  • 1876 Views
  • 4 replies
  • 3 kudos

FatFs f_open() hard fault

int main(void){FATFS FatFs;FIL fil;FRESULT fr;UINT bw; fr = f_mount(&FatFs, "", 0);if (fr != FR_OK) {return (int)fr;}fr = f_open(&fil, "example.txt", FA_WRITE | FA_CREATE_ALWAYS);if (fr != FR_OK) { f_mount(NULL, "", 0);return (int)fr;}f_close(&fil);}...

meco54 by Associate
  • 2063 Views
  • 2 replies
  • 0 kudos

Flashing code with stlink does not run code

I used the STM32CubeIDE to make a simple LED flashing program for an STM32H753. When I run the code with the CubeIDE, it uploads and flashes the LED as intended.I would like to be able to run this code without the CubeIDE. I am on Mac and have stlink...

JKing.8 by Associate III
  • 6084 Views
  • 8 replies
  • 0 kudos