STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

stm32cubeIDE 1.16 errata

Hi,I am developing software on the stm32h743 using threadx and have just updated the IDE to version 1.16.In the Errata document for IDE 1.16 under target specific issues it says the following:184869ThreadX should not be available on H7 single core, a...

alan32 by Associate
  • 2382 Views
  • 2 replies
  • 0 kudos

Resolved! Where to call HAL_ADC_Start_DMA ?

If I call "HAL_ADC_Start_DMA();" outside of while loop, it's not working.If I call it inside the while loop, it's working. /**************************************************************************************Issue in starting multichannel ADC throu...

Screenshot 2024-07-24 102732.png
vijay_66 by Associate II
  • 4822 Views
  • 5 replies
  • 1 kudos

ST OpenBootLoader for stm32g491 on UART1 not work

Hi everyoneusing the UART1 by modifying the tx and rx pins according to my personal application, I am unable to connect with the 7F synchronization byte using stm32cubeprogrammer. Below is the code I modified: /* ------------------------- Definitions...

RS62 by Associate
  • 1109 Views
  • 1 replies
  • 0 kudos

MQTT_VAR_HEADER_BUFFER_LEN

I am trying to send and subscribe data via mqtt protocol using the lwip library with an STM32F207 series microcontroller. When I define MQTT_VAR_HEADER_BUFFER_LEN as 256, I have no problem receiving data. However, when I set MQTT_VAR_HEADER_BUFFER_LE...

Resolved! STM32cubeIDE 1.15.1 no longer available

Hello,I have installed and used STM32cubeIDE 1.15.1 on some workstations, and I want to replicate exactly this development environment on a new workstation.In the downloads page, this version 1.15.1 is no longer available for Linux Debian.Where can I...

JLemi by Associate III
  • 2599 Views
  • 2 replies
  • 0 kudos

Resolved! No ST-LINK detected - NUCLEO-F429Zi board

Hi, I tryed differents issues to solve my probleme, include this :https://stackoverflow.com/questions/72564141/why-is-my-stm32f407-not-being-recognized-by-computer-windows-10 https://stackoverflow.com/questions/71678792/st-link-v2-detected-as-usb-mas...

image.png image.png image.png image.png
mzi by Associate II
  • 3107 Views
  • 5 replies
  • 2 kudos