STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 561 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! About STM32CubeIDE Code Generation

Sorry for the rudimentary question. I tried to generate code by setting up pin assignments in STM32CubeIDE with reference to the following site, but the code such as main.c is not generated as shown in the following image.If you know the cause of the...

CODE01.bmp yunkel_0-1723125440417.png
yunkel by Associate
  • 2564 Views
  • 3 replies
  • 3 kudos

Unable to upload my code using Serial Wire Debug

   I am trying to upload my code using ST Link(SWD)into a custom board with an STM32 Core. I am using serial wire debug for programming. So I am getting the above shown error messages. If anyone have come across this issue, please help me resolve it....

Screenshot 2024-08-05 163011.png Screenshot 2024-08-05 162955.png Screenshot 2024-08-05 162916.png Screenshot 2024-08-05 163741.png
vbk22398 by Senior
  • 11474 Views
  • 23 replies
  • 11 kudos

LVGL and STM32CUBEIDE Integration Issue

I am working with LVGL v9.1.1, I am simulating it correctly in the simulator. When i do all the step of integration with STM32 Project (STM32CUBEIDE v1.16.0). I am getting these errors? why this is been happening. Is this toolchain issue/ any bug? No...

JamshaidUsman_0-1723094091220.png

Touchgfx issue with uart not working good

Hi,I am a beginner to touchgfx, i am using stm32u599vjt6.I am having an issue using uart with touchgfx.My function is to check different conditions every time my handle tick function is called and after checking i need to send some commands from uart...

Accessing IKS4A1 eCompass heading data

Hello,I just recently got into STM32 programming and I have a NUCLEO-F401RE with a IKS4A1 board. I am trying to print the heading data based on the ECompass example so I can eventually send it through UART. For now, I have used Unicleo-GUI to see tha...

Resolved! Downloaded code does not seem to run.

Hello Everyone,I am running CubeIDE on Windows 10. It installed easily and from the little that I know it runs ok.I have the official ST-Link interface for OTHER THAN the Nucleo board and I have upgraded the firmware in there to current release.I hav...

xst by Associate III
  • 3028 Views
  • 5 replies
  • 3 kudos

Resolved! Actual Include paths do not correspond to Include Paths in the settings

Hello, I am trying to add source files in my project, the folder is organized like this : - events :     |  - include :     |      |  - events :     |      |      |  - internal :     |      |      |      |  - Some header files [A]     |      |      |...

Toin_0-1722897384992.png
Toin by Associate II
  • 3481 Views
  • 4 replies
  • 2 kudos

Resolved! STM32 OV2640 DCMI

Hi,I would like to ask a question about STM32 OV2640 usage. My task is; take an output data from OV2640 and send to Computer via USART. When I communicate with UART, I took an output which shown in the figure. I did not is it true or wrong output but...

image.png