STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1417 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! CubeIDE CPP project and Assembly Include

Hello,I have problem with including assembly code into my C++ project.Include section of main.cpp:#include "asm_math_wk.h"asm_math_wk.h file:#ifndef INC_ASM_MATH_WK_H_ #define INC_ASM_MATH_WK_H_ extern void megawkurw(uint32_t test); #endif /* INC_A...

Wikte by Associate
  • 1726 Views
  • 2 replies
  • 2 kudos

Resolved! undefined reference to HAL_TIM* functions

I'm having a problem where the linked complains to me with undefined reference to `HAL_TIM_PWM_Init' erros. The objects that it complains are not defined are HAL TIM based ones such as HAL_TIM_PWM_Init or HAL_TIM_IRQHandler. There is a source file w...

F4 Series SPI HAL Data Size Bug

I am getting a warning during compile of an incompatible pointer type when I call the SPI TransmitReceive function as shown below.Compiler warningI am passing the function an unsigned 16 bit integer array.  I have configured the SPI to use 16 data bi...

STM32CubeIDE F4 SPI_HAL compile warning.png STM32CubeMX_SPI.png STM32CubeIDE F4 SPI_HAL.png

Resolved! VERY weird 'Failed to execute MI command' problem

Hi everyone,   I start to question myself and this whole programming thing....   I'm using a STM32F3-Discovery Board and generated a code with STM32CubeMX in default mode. I changed absolutely nothing before code generation.   In main.c I added the f...

Resolved! How to import an External Tools configuration?

I have created a configuration for use of an external tool (PCLint) and successfully ran the tool in my STM IDE. I exported that configuration and got the .launch file, but now other developers on my team want to run the same external tool configurat...

AO'Do.1 by Associate
  • 4528 Views
  • 3 replies
  • 1 kudos

Resolved! IDE hangs on start - new symptom of sickness ?

This is new "option" on splash screen:!! on top: please close ioc editor --- on startup !!! Nothing is open !!-> Apply and Close --> nothing happens , just (static) splash screen.Is V1.13.1 .Only killing the java process removes the splash screen, bu...

AScha3_0-1706557490496.png AScha3_1-1706558023330.png
AScha.3 by Super User
  • 3158 Views
  • 4 replies
  • 3 kudos

Resolved! help for download this...

i need download this document of this link:https://community.st.com/t5/moderation-archive/cubeide-1-12-cyclomatic-complexity-how-it-works/td-p/71170 but after open link:You do not have sufficient privileges for this resource or its parent to perform ...

kshin.111 by Associate III
  • 975 Views
  • 1 replies
  • 1 kudos

_Noreturn is reported as a syntax error

A syntax error is reported against the _Noreturn specified when a function is declared _Noreturn:_Noreturn void doesNotReturn( void ) { while ( 1 ) ; } The compiler has been configured for C18 and the code compiles.Can I get this to be accepted by ...

CTapp.1 by Senior III
  • 2631 Views
  • 5 replies
  • 0 kudos