STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! CAN id incorrect

I have a STM32G474 mcu that i am learning to program. I have the CANBUS tx on PA12 working by loopback mode. I have connected my logic analyzer and i receive the data correctly.There is only one thing wrong: The ID has bit1 that keeps being set to 1....

PRODNAV by Associate II
  • 6409 Views
  • 10 replies
  • 0 kudos

Resolved! "Nothing to install." after trying to install IDE

I had a problem with the IDE and deleted it by manually searching all the files on my ubuntu 20.04.Now when I try to run the binary again, it says "Nothing to install.", however I have deleted all stm files from my machine.What can I do?

Ksen.1 by Associate
  • 3242 Views
  • 3 replies
  • 0 kudos

Cannot start Manage Embedded software packages

Hallo, I have a problem:STM32CUBE IDE 1.16.0 @ win 7 64bitmyST login - nothing happenedManage Embedded Software Packages - nothing happenedfirmware updater -> Check connection - OKFrom log:!MESSAGE Command 'com.st.stm32cube.ide.mcu.ide.command.userAu...

lkavan by Associate II
  • 1564 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE v1.15 Wrapping read detected

Hello, I am experiencing a bug in STM32CubeIDE since I made the latest update 2 days ago.I was able to download the SW and debug in the previous version, after the updage I can't even download the software using STM32CubeID here is the log :STMicroel...

ABouk.1 by Associate III
  • 2690 Views
  • 3 replies
  • 0 kudos

About STM32F429 ADC value acquisition

Hello everyone, I'm using the STM32CubeIDE , then I would like to ask about the ADC configuration for the STM32F429 board. Currently, I want to distinguish a sine wave input ranging from 10kHz to 3MHz, the ADC parameters are set as follows:(1) APB 1 ...

tasabao by Associate III
  • 4299 Views
  • 8 replies
  • 1 kudos