STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Converting STM32CubeIDE project to Makefile issues

Hello,I've been running into issues porting a simple blinking LED program from STM32CubeIDE to a Makefile based app. I have the exact Drivers (as a submodule that links to the one STM32l0x from github: https://github.com/STMicroelectronics/STM32CubeL...

Pkarra by Associate
  • 2643 Views
  • 0 replies
  • 0 kudos

Undefined references in ThreadX

Hello, I am trying to modify a project from a third party, who gave me a .ioc file. Just the initialization of my board periferics is giving me trouble, as I am a beginner. I keep adding references and driver files, however I don't know which ones I ...

AlbertG by Associate II
  • 1404 Views
  • 1 replies
  • 0 kudos

Resolved! STM32IDE Login problem

Hello, I'm having an issue with my STM32IDE. I just installed it, and when I try to log in, I press the "myST" -> "Login" button, and it opens a box called "User Authentication Dialog," but it's blank, and I can't log in. This is important because ma...

Daniberos_0-1727389645167.png

Resolved! Don't see \core nor main.c in project on STM32Cube

Hello, I am a beginner with STM32IDECube.I have just installed Version: 1.16.1 Build: 22882_20240916_0822 (UTC) which seems to work.I am developing a program with the STM32F107 processor as a target.Everything works so far except that now I want to i...

MDe by Associate III
  • 16639 Views
  • 23 replies
  • 4 kudos

Resolved! Advanced Timer - Input Capture Mode - NVIC Settings

Hello, I using STM32F429IIHX Chip. I wanna use Input Capture Mode, but not working right when i used general timer(tim2,3,5 ...) can use Input Capture Mode. but In TIM8 is advanced mode then, NVIC Settings is a little bit different.  Advanced Timer8 ...

Jdogk_0-1727423700713.png Jdogk_1-1727423718733.png
Jdogk by Associate III
  • 1267 Views
  • 1 replies
  • 0 kudos

Resolved! Multiple definition after update CubeIDE

Hi. Can you say me what mean that type of error.The code is surely correct because I've been working on it. The errors showed up after updating CubeIDE to a new version and generating files from .ioc file in IDE.c:\st\stm32cubeide_1.7.0\stm32cubeide\...

DBrau.2 by Associate III
  • 7744 Views
  • 6 replies
  • 2 kudos

Code Generation would clear my code in `main.c`!

Hi,When I updating the pin assignment information and doing code generation, I find my code, for example, USER CODE part is clear. Why? Is any setup wrong here?   while (1){/* USER CODE END WHILE */ /* USER CODE BEGIN 3 */}/* U STM32CubeIDEVersion: 1...

Fei by Associate
  • 3512 Views
  • 6 replies
  • 1 kudos

STM32CubeIDE search feature not working

Hi Folks,I have the latest version of the IDE (1.16.1) but now the search feature won't work. It will only return an error:When I try to search for "HAL_StatusTypeDef I2C_WaitOnSTOPFlagUntilTimeout" I get the following set of errors:Text SearchAn int...