STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1431 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32 Cube IDE Software Breakpoint

Hi, How to put the software breakpoints in the STM32 Cube IDE. I can put only the hardware breakpoints. The hardware breakpoints has a limitation of maximum 5. We can use multiple software breakpoints in the STM8 Chips with ST Visual Development IDE ...

NM by Associate III
  • 3553 Views
  • 6 replies
  • 1 kudos

Resolved! STM32CUBEIDE install error

It doesn't install as the phrase pops up. "can't initialize plugins directory. please try again later​" I've tried everything. Please help me.window10 64bitintel core i7-6700 3.4GHz

0693W000004Ik7yQAC.png

Resolved! STM32CubeIDE : Firmware installation repository

Updating the program, even for a minor revision like moving from version 1.16.0 to version 1.16.1, the address of the firmware repository is reverted back to the standard.Due to hard disk space limitation I've changed it to a different location, how ...

Max_Cros by Associate
  • 1726 Views
  • 1 replies
  • 1 kudos

CubeIDE doesn't start a workspace on Linux Mint 20.3

Hi,While trying to open a project inside a workspace the CubeIDE stopped loading:As you can see from the log, nothing happen after a while, CPU isn't used at all, and my OS gives me the option to exit the application. You can also see a drop in RAM u...

Captura de pantalla de 2024-03-25 22-16-16.png
XR.1 by Senior
  • 4796 Views
  • 7 replies
  • 6 kudos

I need download 1.6.1

 Hi: I have a code written with ST Cube IDE 1.6.1. I need to add a new characteristic, but with the latest version (1.16.1), the code doesn't compile well.On this link  there is an option to download older versions:https://www.st.com/en/development-t...

j_rios_0-1727903281758.png j_rios_1-1727903315928.png
j_rios by Associate
  • 2688 Views
  • 2 replies
  • 0 kudos

Resolved! How to build a STM32CubeIDE project in a Docker image?

Hi,I am fairly new to the CI/CD processes. I am currently trying to use Bitbucket to run a pipeline to build my STM32CubeIDE project. I have set up the project on Windows in the STM32CubeIDE, I have then setup a pipeline using the image circutor/stm3...

JNoon.1 by Associate III
  • 9677 Views
  • 2 replies
  • 2 kudos