STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1393 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 549 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Handy documents tip for CubeIDE

Hi, I realize I may be teaching Grandma to suck eggs here but I'm a relative newcomer to the STM32 ecosystem and I thought I could maybe help others out with a similar level of experience. Due to the sheer amount of documentation available for ST Mic...

Screenshot 2024-10-01 160007.png

Resolved! undefined reference to '...'

I'm working with stm32h743 MCU on a custom board by myself and stm32cubeide after i generate code without even adding a semicolon to code i build it i get undefined reference for many functions like FreeRTOS,Ethernet and etc and its better to know i ...

Saeedn823 by Associate II
  • 6875 Views
  • 5 replies
  • 2 kudos

Resolved! nothing to build for project STM32446E_EVAL

I have used an example code of CAN loopback using nucleo STM32F446RE the location is C:\Users\.........Your User Name.....\STM32Cube\Repository\STM32Cube_FW_F4_V1.27.1\Projects\STM32446E_EVAL\Examples\CAN\CAN_Loopback Unable to bulid this project and...

Komal by Associate III
  • 8892 Views
  • 10 replies
  • 4 kudos

Page size allocation for malloc

In the STM32CubeIDE predecessor (Atollic IDE) it was possible to set the page size allocation for malloc.Is this somehow also possible in the STM32CubeIDE?Is my understanding correct, that this page size will be reserved from the RAM by the sbrk() fu...

MStuc1_0-1727425781692.png
MStuc.1 by Associate II
  • 2350 Views
  • 5 replies
  • 0 kudos

SBSFU failing to find user firmware

Hi, we are trying to flash with keil mdk bin file and failing when validating user firmware. Below is the output from Tera Term.= [SBOOT] System Security Check successfully passed. Starting...==========================================================...

baymanfl by Associate II
  • 1852 Views
  • 3 replies
  • 0 kudos