STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32G491 Flash memory organization

HelloFor my project I use a stm32g491rct6 with 256k flash. RM0440 Reference manual table 2 say that the flash of this Micro is 256KB in single bank, at this point what is the page size and flash mapping? In stm32g4xx_hal_flash.h FLASH_PAGE_SIZE is 0x...

STM32CubeProgrammer2.17.png STM32CubeProgrammer2.16.png

Resolved! Errors building a project

I made a project with Empty Targeted Project Type and when trying to build the project, it shows an error with the following message:Errors occurred during the build. Errors running builder 'CDT Builder' on project 'HelloWorld'. Internal error buildi...

Can't update ST link

For some reason my I cant update my St link. Issue first came up as debug tool wasnt working properly. Trying again the IDE said no stlink detected when trying to debug the target.    it finds it correctly as shown in the screen shot below (running f...

Screenshot 2024-10-15 204235.png f889c807-880f-4edd-bee5-717aba6eb856.png Screenshot 2024-10-15 204814.png
pingu by Associate
  • 1689 Views
  • 2 replies
  • 1 kudos

How to use GIT branching while using STM32cubeIDE?

Hi all,I have a project that has been developed within STM32CubeIDE. I also have a github repository associated with the project. What I now want to do is branch the project to work on some other features. I may want to have two separate projects in ...

CDyer.1 by Senior
  • 6736 Views
  • 10 replies
  • 6 kudos

Stuck in xQueueSemaphoreTake()

Hi,I would like to setup a system with a telnet server and I'm trying to follow this guide: https://controllerstech.com/stm32-ethernet-4-tcp-server/ but unfortunately, upon launch, the system gets stuck at line1438 in queue.c:/* Cannot block if the s...

debug by Associate III
  • 7040 Views
  • 10 replies
  • 0 kudos

Resolved! STM32CubeCLT Build Issue

Hi, I have a server in AWS which I want to use to build and release my firmware. I installed v1.16.0 on my system as well as on the server. I cloned the project on both the systems and build is successful on my system. But, on the server, I am gettin...

SBhon.1 by Associate III
  • 2799 Views
  • 4 replies
  • 0 kudos

Incremental saving

Hi allWhen I work on project, I like to save everything incrementally maybe 3 or 4 time a day just to be safe . And if I do something "crazy", as program goes bigger and bigger, it easy to revert back to an older project name.If I have my project nam...

Dany0 by Associate II
  • 1459 Views
  • 2 replies
  • 2 kudos