STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Loading code on STM32U535 vs STM32U545

Hello, we have an STM32CubeIDE project based on the STM32U545. Unfortunately, our first version of PCB's is due to arrive soon populated with the STM32U535 instead, due to parts shortages. My question is, can I use the IDE to load and debug the code ...

CSmit.4 by Associate II
  • 1248 Views
  • 1 replies
  • 2 kudos

Resolved! Bug: Annoying GUI Behaviour: Child Windows Disappear

I'm not sure if this is the right forum for this but here goes.When operating with STM32CubeIDE, and doing something that causes a child window to pop up, the window can disappear behind other windows and alt-tab can't find them.  I have to drag othe...

AMacd.1 by Senior
  • 1818 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H573 Debugging in CubeIDE not working

Hi, I'm having issues debugging my custom STM32H573 board.It used to work, before restoring my laptop to factory settings and reinstalling the IDE. I hope someone can help me with the situation, I don't know what fixes to try anymore. Setup: Custom b...

gnarrf95 by Associate
  • 4385 Views
  • 2 replies
  • 3 kudos

Where to report CubeIDE bugs?

Hello,I've updated my STM32CubeIDE to the latest version (1.13.1) and verified that some annoying bugs are still there. I'm curious is there a dedicated place where to report them?I'm talking about really a basic functionality which should be working...

kgardas by Associate III
  • 2836 Views
  • 4 replies
  • 3 kudos

embbeded stm32f746 nucleo board ethernet use

stm32 nucleo board use ethernet communiction  send string on board pb7 led on same off string It looks like you're trying to implement a TCP client on an STM32 Nucleo board that controls an LED connected to pin PB7 based on the string send  on  sever...

Resolved! Problems with Firmware Library Package Setup

Hi,on a brandnew PC with Win10 i installed CubeIDE 1.16.1.After that, i want to import example project "BLE_HeartRate. Then i got this message:  I thougt that CubeIDE installed the required Firmware Package automatically?

2024-10-10_17h49_00.png
ledi001 by Senior
  • 1126 Views
  • 1 replies
  • 0 kudos

regular HAL_RTC WakeUp

Hello,I'm testing the PWR_STOP_RTC sample on STM32L0538-Discovery.I see how to wake-up period with WakeUpCounter in  the function HAL_RTCEx_SetWakeUpTimer_IT().I think I'd generate periodical wakeup interrupt with fixed period.Is  there any specific ...

curiae by Associate III
  • 988 Views
  • 1 replies
  • 0 kudos

Cannot activate IRTIM peripheral

Hi, I'm developing an application based on STM32U031K8. I need to use the IRTIM peripheral to create an IR transmitter. I set TIM15_CH1 and TIM16_CH1 as "Output Compare No Output" but IRTIM peripheral still cannot be activated. May someone help me?

aerauliqa by Associate II
  • 3287 Views
  • 8 replies
  • 0 kudos