STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1426 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32H755 CM4's HAL_Delay() never returns

Hi All,I have a problem on H755 Nucleo which is that the M4's tick doesn't seem to be advancing.Digging a little deeper I can see that uwTickFreq is zero, but I can't see why that's happened. There must be something wrong in my .ioc file since I've h...

bramble by Senior
  • 1769 Views
  • 5 replies
  • 0 kudos

Resolved! Generating .srec file from command line

Hey,I am using the STM32f769NIH controller and my application has Touchgfx and freeRTOS enabled. The code downloading time is too slow and I want to speed it up.I figured that turning off the external loaders in the debug configurations yields a smal...

CubeIDE problems

Hi boys and girls from ST,I am testing your CubeIDE and it it catastrophe.1/ I tried to open a new project in CubeID and I ascertained that I can not add assembly file (s). How I can create project with only one file - in assembly. :)2/ I tried to cl...

JerryMC22 by Associate III
  • 3864 Views
  • 4 replies
  • 3 kudos

STM32F439ZI ETHERNET TCP CONNECTION

Hi,I am using stm32f439zi eval board for TCP communication. I can ping the board from host. It shows TCP connection error in Hercules utility. I am using port number 7 to listen to server. I am not sure whether I am using correct port number for the ...

arun27 by Associate II
  • 1020 Views
  • 1 replies
  • 1 kudos

Segger J-Link STM32H755 CM4 debugging in STM32CubeIDE

I am trying to debug the STM32H755 within CUBEIDE but the current segger J-link drivers say that core is not supported. The segger website lists it as supported and it works without issues in their debuggers.I am wondering if there is a workaround or...

Ckerl.2 by Associate II
  • 2187 Views
  • 4 replies
  • 0 kudos

Ubuntu 22.04 CubeIDE either freezing or no IOC editor

I was having this problem https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-user-interface-freezing-in-ubuntu-22-04-wayland/td-p/656993 so I tried the solution and it fixed the freezing, but now the IOC editor doesn't render, such as with ht...

DShekter by Associate III
  • 2128 Views
  • 5 replies
  • 1 kudos

STM32CubeIDE 1.14.1 Login to myST does nothing

With STM32CubeIDE 1.14.1 running on Windows10 the login to myST does not work anymore. Clicking the menu item or using the hotkey Alt-L simply does nothing - no reaction, no error message, NOTHING. It worked some time ago but all of a sudden does not...

MSchm.1 by Associate II
  • 8415 Views
  • 17 replies
  • 3 kudos