User Activity

Hello everyone,I've just updated cubeIDE from V1.14.x to V1.15.1 and duration of build process on the same project increased by around 4x.  With V1.14 it took around ~10s, now with V1.15.1 takes ~40s to build the same project on the same machine.  Is...
Hello everyone! BackgroundWe are working on STM32G474VET6 based custom board for some specific motor control application. Project demands to have a custom bootloader on FD-CAN with 500kbit/s arbitration baudrate and data rate with 2Mbit/s with BRS op...