STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1471 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 571 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Ethernet_F439_Error_Handler

 I am using a standard working example of STM32F429ZI on an STM32F439ZI. Usually if the pinout match, these codes work if the series differs also. But the Ethernet initialization is not happening and since the code is given by STM32 Cube IDE, unable ...

Screenshot 2025-01-09 105141.png

RTOS Aware Debug

IDE VERSION: v1.14.1+Target: STM32H750Debugger: ST-LinkSo, 98.9% of the time I try to enable RTOS aware while debugging using the ST-Link I receive this message:After that, I'm no longer able to debug code. This is normally "worked around" by closing...

rmartins_0-1741035795145.png
rmartins by Associate II
  • 1108 Views
  • 2 replies
  • 0 kudos

Resolved! Issue with Code Generation in STM32CubeIDE for STM32H747

Hi everyone,I'm working on a project with STM32CubeIDE and an STM32H747 microcontroller. I've configured the clock sources in the .ioc file as follows:High Speed Clock (HSE): BYPASS Clock SourceLow Speed Clock (LSE): Crystal/Ceramic Resonator  When I...

SSerg4_0-1741119975325.png
SSerg.4 by Associate III
  • 1370 Views
  • 2 replies
  • 1 kudos