STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1431 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32F767 DTCM cache - static variables

Hello,i have enabled D-cache and I-cache and im trying to place static variables into D-cache:   __attribute__((section(".dtcmram"))) __attribute__((aligned(32))) static float32_t FFTOutput_average[MAX_FFT_PRINT_SIZE] = {0};   I updated linker script...

Petr3 by Associate III
  • 2435 Views
  • 6 replies
  • 0 kudos

Resolved! utf16 file encoding in CUBEIDE

Hi,I have a c++ file with a table of utf16 c style strings encoded as utf16. I need this file to be encoded as utf16 for the compiler to understand correctly the 'special' characters. In IAR, it was super easy as the compiler could read both utf8 and...

GMeur by Senior II
  • 1132 Views
  • 1 replies
  • 1 kudos

Ethernet_F439_Error_Handler

 I am using a standard working example of STM32F429ZI on an STM32F439ZI. Usually if the pinout match, these codes work if the series differs also. But the Ethernet initialization is not happening and since the code is given by STM32 Cube IDE, unable ...

Screenshot 2025-01-09 105141.png