2024-10-16 6:28 AM
Hi all, I've a question.
I created a new project and there I linked externally some user made modules with the command Import (Right click kn project name, then choose import, add the wanted modules and linked them into the project).
I try to compile and everything was ok.
Now my question: I need to exclude some files from compiling process, both in debug and release mode. I was able to exclude them by the command "Resource Configuration" but when I delete and import again the modules, and link them again to the project, I see that the compiling filters has been restored to default values meanwhile I need to keep the filters on everytime.
There is a way to achieve this?
2024-10-16 7:30 AM
Hello @zioMorgan
First let me thank you for posting.
Try to follow these steps , you can manage file exclusions more effectively in STM32CubeIDE:
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.