STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1409 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Print in stm32cubeIDE using st link

Hi, I'm using an STM32F103C8T6 blue pill board with st link programmerand I want to print a single string hello world Can we do that with st link or we do need something else to do it ?thank you for helping

Abdegou_8 by Associate II
  • 2592 Views
  • 3 replies
  • 2 kudos

STM32CubeIDE can't find DSP static library

HiiI have a problem when I add ARM DSP library, the following error appears:c:\st\stm32cubeide_1.0.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld....

0693W000000V6PiQAK.jpg 0693W000000V6PYQA0.jpg 0693W000000V6PTQA0.jpg 0693W000000V6POQA0.jpg

Resolved! Files for STM32H563 External Loader

Anybody have Linker.ld and Loader_src.c file for STM32H563?  I have done one for the STM32H743 on another project and made an attempt to modify these for the STM32H563 but it's not working.  Appreciate any guidance.I changed the RAM location from 0x2...

PFlor.2 by Senior II
  • 7589 Views
  • 10 replies
  • 1 kudos

Using tracealyzer with threadX

Hi, I am trying to use threadX with tracealyzer. I am following https://percepio.com/getstarted/latest/html/threadx.html.but upon compiling, I am getting the following reference errors:../Middlewares/ST/threadx/common/src/tx_byte_allocate.c:410: unde...

Guru93 by Associate
  • 961 Views
  • 1 replies
  • 0 kudos

Resolved! stm32u5 OpenOCD and stlink-server issues on macOS

I am trying to connect to the b-u585i-iot02a on macOS 15.3.1 using OpenOCD without success. The same board, cables and configuration scripts with the same version of OpenOCD (0.12.0+dev-01888-ga168c6341) works on both Windows 11 and Ubuntu 24.04. ST-...

larschrj by Associate
  • 2104 Views
  • 2 replies
  • 2 kudos