STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 220 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

Resolved! How to run BLE examples on STM32WB55 Nucleo?

I have downloaded the stm32cube package that contains the BLE example but i am unable to correctly import and run any of the project on the MCU.Looking for help, thank you.

HIfti by Associate II
  • 2105 Views
  • 4 replies
  • 0 kudos

Does the B-L072Z-LRWAN1 support I2C in both slave/master mode.

I wish to connect this kit (STM32L072CZY6TR) to a raspberry pi. As the Pi only supports SPI in master mode I need to use I2C to get a two way conversation. I wish to send and receive the occasional codes from a server via LORAWAN and communicate thos...

JAnth by Associate
  • 984 Views
  • 1 replies
  • 0 kudos

STM32WB55 BLE Stack can't work on stm32wb55RGV6

Hi All, I have trouble getting the BlE working on my new hardware(stm32wb55RGV6). The prgram can't enter into  APP_BLE_Init( ); . The same code in P-NUCLEO-WB55.Nucleo(stm32wb55RGV6U)can work. What's different between stm32wb55RGV6  and stm...

Htzuh by Associate II
  • 4186 Views
  • 10 replies
  • 0 kudos

Resolved! STM32WB55 Nucleo - unexpected current consumption in STOP2 mode

Hello,I used the Nucleo STM32WB55 board to test the STM32WB55xx current consumption.I took the PWR_STOP2_RTC example from the STM32Cube MCU package for STM32WB Series (v1.2.0)With STM32CubeMx v5.3.0 I re-generated code for Truestudio (I am using True...

JBron by Associate II
  • 4349 Views
  • 7 replies
  • 0 kudos

How to get a timestamp for my end node which is a STML082?

I need to know, is there any specific command(Like a AT Command) to get a timestamp from any network server or gateway for the end device STML082? Is there any API we can find in the "STM32 Cube Expansion" stack to implement it? If there, then where...

GBehe by Associate III
  • 768 Views
  • 0 replies
  • 0 kudos