NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
The Murata module connects to another MCU which has bluetooth. I want the update to go over bluetooth and write it to the module with AT commands.
Hello!I'm going to build an application in Java for Iphone and Android using GluonHQ framework. The application should logging values from a STM32 board. I have a STM32f401RE board and STM32f446RE board. I want to implement FreeRTOS on them and then ...
Hi everyone,I just finished a project with the cubeLRWAN example and it works well. But I have a question. In many tutorial I saw that people put an mspInit() after stop mode but not before. Why do we not initialise the card the same way before and a...
Hello community,I'm getting started with the STM32WB55 Nucleo board and worked through some examples. To get a better understanding I chose to start a new project from scratch. I used CubeIDE (came from Atollic TS and CubeMX anyways) and initalised t...
Hi everyone,I am using the Nucleo-WB55RG to try and fully erase/program the flash memory. However, when the FLASH_MassErase() function is called in stm32wbxx_hal_flash_ex.c, a hard fault exception occurs. I believe this has to do with trying to erase...
Hi, i am making some tests with my BL072Z board, with SF7 uplinks and downlinks are ok, but when y run the code with SF12 i only can send uplinks, in TTN i can see the scheduled downlink and in the next uplink the downlink is sent but in the BL072Z b...
I am trying to understand what parameters I could change to increase throughput. In the file app_conf.h/** * Maximum supported ATT_MTU size */ #define CFG_BLE_MAX_ATT_MTU (156) /** * Size of the storage area for Attribute values * ...
I am using the STM32CubeIDE and using my new P-NUCLEO-WB55. I have tried to create a simple project and ran a debug session but it is always getting stuck in Hard Fault Error. Please find the attached screenshot.
I just started working on STM32WB55 and was going through the BLE example codes given in the STM32Cube_FW_WB_V1.2.0 package. I am confused in understanding the program structure of the code (where to add new services, characteristics, where to handle...
i'm trying to use the Nucleo WB55 dongle as a mass storage device.Using cubeMx i set the USB, and the USB Middleware as MSC, leaving the default settings. Nothing else is running on the dongle, just USB.When i plug it, it appear as an unknown device....