STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

Cannot flash nucleo_wb55rg using west.

I get this errorc:\Users\sabdalla\zephyrproject\zephyrproject\zephyr>west flash-- west flash: rebuildingninja: no work to do.-- west flash: using runner pyocd-- runners.pyocd: Flashing file: C:/Users/sabdalla/zephyrproject/zephyrproject/zephyr/build/...

SAbda by Associate
  • 803 Views
  • 0 replies
  • 0 kudos

Resolved! What is the difference between STM32WB55 and ES32WB55?

Hi, I have two types of MCUs that I am building a board with. One is labeled as STM32WB55, while the other one is ES32WB55. Is there any difference between the two? I could not find any information on the ES32 chip in my Googling. I am having trouble...

e.li1 by Associate
  • 1548 Views
  • 3 replies
  • 0 kudos

Resolved! HAL_SAI_Receive_DMA doesn't start the DMA

Platform: STM32WB55 discovery board connected to I2S codec.My mission: To receive data from the codec using DMA transfer.Calling to HAL_SAI_Receive function returns the data correctly so I guess that everything is configured correctly.When calling to...

ELaha by Associate
  • 2469 Views
  • 3 replies
  • 0 kudos

How To Connect Your First LoRa Device ( STM32L072CZ Microcontroller ) Using B-L072Z-LRWAN1 And The Shield X-NUCLEO-IKS01A2 From STMicroelectronics

Hello , Today I Wrote My Second Article Entitled How To Connect Your First LoRa Device ( STM32L072CZ Microcontroller ) . In This Project i used The B-L072Z-LRWAN1 Development Board From STMicroelectronics and Also the Shield X-NUCLEO-IKS01A2 From STM...

Resolved! RTC clock ticking faster than actual.

Hello everyone,I am currently developing a code for my custom board that has BLE communication along with RTC and timer(PWM) initialized. I am currently testing my code first on the PNucleoWB55 development board. The issue is that the normal RTC_Alar...

AKetc by Associate III
  • 4032 Views
  • 5 replies
  • 0 kudos

Resolved! Why I can't received a message downlink immediately?

Hi All;​ I am use I-CUBE-LRWAN version 1.2.1. I am program in class C mode. I send a message downlink from network server and I checked that the data was actually sent out. Why I can't received a message downlink immediately. Could you please adv...

Gz by Senior
  • 1087 Views
  • 1 replies
  • 0 kudos