User Activity

Hi,I know that the question may seem silly (if devices are non-discoverable they should not be reported in a BLE scan result) but it looks like it is more complicated than that.I am using STM32WB55 MCU.I need to scan for BLE beacons that are around m...
Hi,I have downloaded the STSW-BLUETILE-DK 1.2.0 package and I am trying the build the examples (for instance the BLE_SensorDemo within Project/BLE_Examples directory) on Truestudio.I get the following error:In file included from ../../../src/BlueNRG1...
Hello,I used the Nucleo STM32WB55 board to test the STM32WB55xx current consumption.I took the PWR_STOP2_RTC example from the STM32Cube MCU package for STM32WB Series (v1.2.0)With STM32CubeMx v5.3.0 I re-generated code for Truestudio (I am using True...
Kudos from