STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

STM32WB55 BLE Security

Hi,Is there any example/Demo available which represent complete BLE security. i.e Paring using numeric comparison method and also only authorized person can read or write BLE characteristics.How we can implement such kind of security in stm32wb55. Pl...

asala.19 by Associate III
  • 2483 Views
  • 3 replies
  • 0 kudos

STM32WB Fixed Advertising Channel for Certification

Hey Guys,I have a problem with my STM32WB55CC. For the certification of my product I have to set the advertising channel to a fixed one (37, 38, 39). The command I try to use is the following:volatile uint8_t ret; ret = hci_le_set_advertising_paramet...

BSpoe.1 by Associate III
  • 3158 Views
  • 6 replies
  • 0 kudos

Unable to flash my P-NUCLEO-WB55 dongle

Using DFU. I repeatdly try to flash the dongle, it almost always fails and when it seems to start erasing prior to writing it ends up with :$ ./STM32_Programmer_CLI -c port=usb1 -d /tmp/BLE_p2pServer_reference.hex      -------------------------------...

ODEBO.1 by Associate
  • 1621 Views
  • 2 replies
  • 0 kudos

STM32WB55 USB DONGLE debugging via USB not working

Hello,I am a newbie and trying to get debugging on my STM32WB55 USB Dongle Board to work.I have LPUART1 and USART1 set up, but don't understand what else is required to set up?Is there any example project for the USB Dongle Board using the USB conne...

MHell.1 by Associate II
  • 959 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to find AN 5500

Hi,where can i find AN5500: ZSDK API for ZigBee® on STM32WB Series, referenced in AN5492 to be available on www.st.com?Regards, Rainer

Rainer1 by Associate III
  • 3704 Views
  • 3 replies
  • 0 kudos

– Integrated balun to reduce BOM

we are using ble in stm32wb series – Integrated balun design is there any reference schematic .the height of our application is 40feet can we use this ble with balun anteena or we will need an external antenna who we calculate the range and power ?

MRajn by Associate
  • 1025 Views
  • 1 replies
  • 0 kudos

STM32WB - Problems with BLE and RTC

Hey Guys, Im new to ST and have the following Problem with the STM32WB55.I want to use the BLE function while the RTC is running in the background. The BLE should run for 10 seconds and shutdown after for 1 minute.When I go into the Standby Mode (Wit...

MLind.2 by Associate
  • 1024 Views
  • 0 replies
  • 0 kudos

STM32WB55 BLE Beacon Example doesn't work

Hi all,i bought the STM32WB55 Nucleo Pack and I tried different examples from the STM32WB55 Firmware Package. The BLE Datathroughput example worked fine for me, but the BLE Beacon won't work.I updated the FUS to the newest version.I flashed the newes...

PNeub.1 by Associate
  • 1493 Views
  • 1 replies
  • 0 kudos