STM32WB - Problems with BLE and RTC
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-05-25 7:26 AM
Hey Guys, Im new to ST and have the following Problem with the STM32WB55.
I want to use the BLE function while the RTC is running in the background. The BLE should run for 10 seconds and shutdown after for 1 minute.
- When I go into the Standby Mode (Without BLE), i have a power consumption arround 800 nA, which is fine. When i'm doing this after I initialized the BLE with the "APPE_Init();", my power consumption is arround 0.6 mA, which is far to much. How can i fix this?
- Can i use the BLE without effecting the RTC? I saw that the BLE is using the RTC clock and also changes the prescaler.
Thanks a lot!
Labels:
- Labels:
-
BLE
-
RTC
-
STM32WB series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0