cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB can not understand "shci_init(APPE_SysUserEvtRx, (void*) &SHci_Tl_Init_Conf)"

zxin.2116
Associate II

code from V1.3 :

UTIL_SEQ_RegTask( 1<< CFG_TASK_SYSTEM_HCI_ASYNCH_EVT_ID, UTIL_SEQ_RFU, shci_user_evt_proc );

 SHci_Tl_Init_Conf.p_cmdbuffer = (uint8_t*)&SystemCmdBuffer;

 SHci_Tl_Init_Conf.StatusNotCallBack = APPE_SysStatusNot;

 shci_init(APPE_SysUserEvtRx, (void*) &SHci_Tl_Init_Conf);

in shci_user_evt_proc function:

 if (shciContext.UserEvtRx != NULL)

  {

   UserEvtRxParam.pckt = phcievtbuffer;

   shciContext.UserEvtRx((void *)&UserEvtRxParam); 

   SHCI_TL_UserEventFlow = UserEvtRxParam.status;

  }

and the APPE_SysUserEvtRx:

static void APPE_SysUserEvtRx( void * pPayload )

{

 UNUSED(pPayload);

 /* Traces channel initialization */

 TL_TRACES_Init( );

 APP_BLE_Init( );

 UTIL_LPM_SetOffMode(1U << CFG_LPM_APP, UTIL_LPM_ENABLE);

 return;

}

if the shci_notify_asynch_evt do,

void shci_notify_asynch_evt(void* pdata)

{

 UTIL_SEQ_SetTask( 1<<CFG_TASK_SYSTEM_HCI_ASYNCH_EVT_ID, CFG_SCH_PRIO_0);

 return;

}

I am hard to understand ,when the " shci_user_evt_proc " do ,the APPE_SysUserEvtRx wil do, the initial will do ?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0