STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

[STM32WB55] BLE + HID?

When generating a new project (cubemx 5.5.0) that includes HID and BLE.I rebuilt the sample apps provided by STM for each of these features and they work OK. However I have no clue as to how to combine the two (most probably because I'm setting the c...

PMera.1 by Associate III
  • 6681 Views
  • 15 replies
  • 0 kudos

STM32WLE5J8/JB/JC LoRa RF (antenna) circuit reference

Hi, I am looking for reference design for STM32WLE5J8/JB/JC LoRa SoC.I found reference for NUCLEO-WL55JC board but was not able to find it on ST micro website.I also want to check if its possible to design 2x wireless circuit (415MHz and 865MHz) usin...

SRaj.1 by Associate II
  • 1971 Views
  • 3 replies
  • 0 kudos

I have a Bluetooth eval board, the STEVAL-IDB007V1M, and I would like to do a quick operational check with my Win10 laptop.

I have downloaded TERA-TERM to my laptop but it sees nothing. Furthermore I can see no activity on any signal line (UART,SPI or I2C) to the SPBTLE-1S Bluetooth module. I presume SPBTLE-1S would be driven by the host MCU whether or not there is a rece...

JCHRI.1 by Associate II
  • 724 Views
  • 0 replies
  • 0 kudos

Is a STM32F4xx library compatible with STM32L072C7?

I bought a B-L072Z-LRWAN1 with STM32L072C7 as the processor and a NEO 6M GPS module. I found a library on this site https://stm32f4-discovery.net/2014/08/library-27-gps-stm32f4-devices/ Is the TM STM32F4 GPIO Library compatible with my board?

ppete.1 by Associate II
  • 719 Views
  • 0 replies
  • 0 kudos

Resolved! Odd response when sending FUS (0.5.3) command

I'm using a custom board with a STM32WB50CG part. When I send this:0x10 0xFC 0x52 0x00 (FUS_GET_STATE) or any command for that matter, I always get this back:0x11 0x0E 0x04 0xFF 0xFE 0x00 0xFE 0x00I've tried this while running the bootloader code as ...

Eric1 by Associate II
  • 2059 Views
  • 4 replies
  • 0 kudos