cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to flash my P-NUCLEO-WB55 dongle

ODEBO.1
Associate

Using DFU. I repeatdly try to flash the dongle, it almost always fails and when it seems to start erasing prior to writing it ends up with :

$ ./STM32_Programmer_CLI -c port=usb1 -d /tmp/BLE_p2pServer_reference.hex

     -------------------------------------------------------------------

                       STM32CubeProgrammer v2.4.0                 

     -------------------------------------------------------------------

USB speed  : Full Speed (12MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : STMicroelectronics

SN         : 2057387B3136

FW version : 0x011a

Device ID  : 0x0495

Device name : STM32WB55xx

Flash size : 1 MBytes

Device type : MCU

Device CPU : Cortex-M0+/M4

Memory Programming ...

Opening and parsing file: BLE_p2pServer_reference.hex

 File         : BLE_p2pServer_reference.hex

 Size         : 17841 Bytes

 Address      : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 4]

erasing sector 0000 @: 0x08000000 failed

erasing sector 0001 @: 0x08001000 failed

erasing sector 0002 @: 0x08002000 failed

erasing sector 0003 @: 0x08003000 failed

erasing sector 0004 @: 0x08004000 failed

Download in Progress:

Error: failed to download Segment[0]

Error: failed to download the File

Previous attempts fails with "unsupported" command for this device, or asking for -rdu.

When -rdu is invoked it randomly telling me that RDP is 0xBB where it reads out 0xAA (no protection).

Help

-Olivier

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Rainer1
Associate III

Have you tried to use the GUI Version 2.4.0? A far as i am concerned, it works more reliable than the cli version.

ODEBO.1
Associate

Thank you for your reply. I actually switched to CLI because the UI tool was behaving inconsistently. I had no issues with the Nucleo board so I concluded that the DFU part of the tool is just crappy. It works better (though not reliably) on Windows (7 here), and I could get the FUS, Stack and application downloaded properly to the dongle. This is surprising since it's a Java tool. Well I guess the serial port part is obviously not common to both platforms (Java has no good solution for this).

Since Windows is a no go for me, I think I'll use standard dfu tools on Linux or stick with the Nucleo dev board instead of the dongle.