STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

Why are closed MX projects still being processed?

To focus on one project I close all the other projects.But still by pressing CMD-B (Mac) all MX-projects get rebuild.The closed MX-projects can still be collapsed/uncollapsed.Search ...Problems Tab ...This very time consuming.I think this should not ...

Mistake in RM0434 (STM32WB) in IPCC description

I found a mistake in RM0434 in IPCC description.Figure 399 IPCC Simplex - Send procedure state diagram.After the rectangle with "UNMASK Channel N free interrupt" should be "Write CHnFM = 0" instead of "Write CHnFM = 1"Thanks.

I-NUCLEO-LRWAN1 and STM32F767ZI problem with usart

Hi, I'm working on the Lora project. I have a STM32F767ZI board and an I-NUCLEO-LRWAN1 module. As I understood from the manual to the module. The module is programmed using AT commands via UART. I set up USART3 on my board to communicate with a PC th...

DJeze.1 by Associate II
  • 3614 Views
  • 8 replies
  • 0 kudos

help with stm32WB BLE

Hello,I am a beginner with ble. I have worked with other stm boards in the past. I need help with the STM32WB baord.I used cube mx to generate the start up code. Enabled rf, rtc and everything.Enabled custom template in server modeadded a service and...

HPate.6 by Associate
  • 994 Views
  • 0 replies
  • 0 kudos

HardFault in the workshop on blue thooght with 03-STM32W-WS__How_to_add_BLE_functionality_V2.2. I can turn on and off the blue led. When I press button 1, the cortexM4 goes well in the interrupt routine: void HAL_GPIO_EXTI_Callback.

After the Return instruction, the Cortex M goes into Hardflault.I use the STM32CubeIder 1.5.1.. It uses sequencer.c. I attach two screen prints:The:void HAL_GPIO_EXTI_Callback, where there is a breakpointand that of the fault analyzer:

0693W000007DbYOQA0.png 0693W000007DbbrQAC.png