STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32wb Unable to start the advertising

Hello Geeks!I'm playing with STM32WB.Actually, I'm using in one of our product as an SOCI'm using the Former version of the Cube packages, i guess "1.7.x"As we all know, the former version of the Cube packages was unstable and almost impossible to pl...

STM32WB55xx STM32WB35xx BLE 5.0 minimum required time for maximum throughput. Connection is getting lost during the transfer of data more than 100Kbytes.

Hello We are using STM32WB55xx STM32WB35xx Nucleo board with STM Ble stack. We want to transfer data around 2Mbytes after connection.After connection, we are only able to transfer around 100Kbytes of data after that connection is getting lost.What i...

Jagath by Associate II
  • 612 Views
  • 0 replies
  • 0 kudos

Resolved! ADC: Cannot change channel.

Board: STM32WB55-NUCLEO PackI am unable to change the channel being read by the ADC using the included code. I have set the number of conversion to 3 in the ADC configurations. I am not using the DMA but am polling. uint32_t get_battery_voltage(){  ...

TomC by Senior
  • 3516 Views
  • 6 replies
  • 1 kudos

PLL, cannot reach 48-MHz

Dear all,I am trying to set-up the internal PLL for running @ 48-MHz.I can easily set-up the clock tree to achieve frequencies lower than 44-MHz, but when I try 48-MHz, the cpu does not end from the loop that verify that the PLL is OK.The FLASH is se...

EFran.1 by Associate
  • 697 Views
  • 0 replies
  • 1 kudos