User Activity

I am an owner of the STEVAL-EDUKIT, an inverted pendulum kit by ST with an NUCLEO-F401RE, IHM01A1, Nema17 motor and an rotary encoder + a 2A, 12V power supply. I have no prior experience with motor control whatsoever. See https://www.st.com/content/s...
I had a working project in STM32CubeIDE when "suddenly" HAL_Delay() did no longer properly work (with the stepper motor shield). During investigation I found that HAL_Delay was basically hanging forever. No, without knowingly changing something, my c...
I am using a IHM01A1 Stepper motor shield with an STM32F401. The provided example for one motor from the X-CUBE-SPN1 package works as expected and I can properly control the motor.Now I want to basically recreate the project from scratch as a prober ...
I just assembled my EDUKIT01 and getting my feet wet. I downloaded all the available PDFs, files, etc. from https://www.st.com/content/st_com/en/campaigns/educationalplatforms/motorcontrol-edu.html and also from the https://sites.google.com/view/ucla...
The example "DAC_SignalGenerator" is not working as expected for me using a NUCLEO-WL55JC1 board. Using CubeIDE 1.6 with FW Pack 1.0Using the on board button one should be able to switch between a triangle and a "escalator" waveform. While the triang...
Kudos from