STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

NUCLEO-55WLJC1: Most Elemental HAL Functions Don't work

Hey guys, I'm Working on the NUCLEO-55WLJC1 Board. My Problem seems very simple but I've been struggling with this for some time now. I want to use HAL_GPIO_TogglePin To toggle a pin, but it has no effect at all. I tried to use HAL_GPIO_WritePin inst...

0693W000007EKhuQAG.jpg
MSchn.3 by Associate II
  • 1071 Views
  • 1 replies
  • 0 kudos

Defined Pins float on about 0.7 V

My pins seem to just be floating even though, i have set them to specific levels.the only one, that works properly is Pin 3 on 3.3 V. MX_GPIO_Init(); /* USER CODE BEGIN 2 */ HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, GPIO_PIN_RESET); HAL_GPIO...

MSchn.3 by Associate II
  • 1455 Views
  • 3 replies
  • 0 kudos

Resolved! STM32WB BLE Connection examples v1.10.0

Hi,i have an STM32WB used as client. Compiling the project with libraries 1.8.0 i can connect 5 BLE servers without any problem, compiling the project with libraries 1.10.0 i can't connect more than 2 BLE Servers, from the third aci_gap_create_connec...

LSpad.1 by Associate III
  • 1277 Views
  • 1 replies
  • 0 kudos